k60 USB0 settings

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
2,170件の閲覧回数
bataliero
Contributor III

cpu

 

My cpu settings : I use PLL and 8MHz external crystal

but when I try to use USB - error occurs:

" No timing clock signal for device USB0 (FLL is disabled in the PEE MCG mode. See 'MCG settigns/FLL settings' of the 'Clock source setting 0' used by the 'Clock configuration 0' in cpu component.) "

 

 

How to turn USB  on?

 

 

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
1,915件の閲覧回数
MVa
NXP Employee
NXP Employee

Hi,

  switch to the "Expert" view and  in the "Cpu" component select "PLL clock" value in the "PLL/FLL clock selection" property (see attached picture).

 

MVa

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,916件の閲覧回数
MVa
NXP Employee
NXP Employee

Hi,

  switch to the "Expert" view and  in the "Cpu" component select "PLL clock" value in the "PLL/FLL clock selection" property (see attached picture).

 

MVa

0 件の賞賛
返信