inflate returned -3

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

inflate returned -3

2,440 次查看
madhukumar
Contributor I

Hello,

During the booting process error occurred it shows inflate returned -3, the kernel console output as shows below, please give suggestion

U-Boot 1.3.3 (Apr 16 2015 - 12:05:58)

CPU:   Freescale MCF5485

       CPU CLK 150 Mhz BUS CLK 75 Mhz

Board-->u-boot.bin-V1.0

SATTVA etech Himagni CPU Board

DRAM:  64 MB

FLASH:  8 MB

In:    serial

Out:   serial

Err:   serial

Net:   FEC0, FEC1

Hit any key to stop autoboot:  0

## Booting kernel from Legacy Image at ff850000 ...

   Image Name: Linux Kernel Image

   Image Type: M68K Linux Kernel Image (uncompressed)

   Data Size: 2244608 Bytes =  2.1 MB

   Load Address: 00020000

   Entry Point: 00020000

   Verifying Checksum ... OK

   Loading Kernel Image ... OK

OK

Linux version 2.6.25 ([email protected]) (gcc version 4.4.1 (Sourcery G++ Lite 4.4-217) ) #22 Thu Nov 22 16:10:35 IST 2012

starting up linux startmem 0x27c000, endmem 0x4000000,          size 61MB

console [ttyS0] enabled

Built 1 zonelists in Zone order, mobility grouping on.  Total pages: 8156

Kernel command line: root=/dev/mtdblock1 rw rootfstype=jffs2 mtdparts=physmap-flash.0:2560k(kernel)ro,5376k(root) console=ttyS0,19200

PID hash table entries: 256 (order: 8, 1024 bytes)

Console: colour dummy device 80x25

Dentry cache hash table entries: 8192 (order: 2, 32768 bytes)

Inode-cache hash table entries: 4096 (order: 1, 16384 bytes)

Memory: 62592k/62592k available (1672k kernel code, 1200k data, 64k init)

SLUB: Genslabs=13, HWalign=16, Order=0-2, MinObjects=8, CPUs=1, Nodes=1

Mount-cache hash table entries: 1024

net_namespace: 152 bytes

NET: Registered protocol family 16

MCF5485x INIT_DEVICES

NET: Registered protocol family 2

IP route cache hash table entries: 2048 (order: 0, 8192 bytes)

TCP established hash table entries: 2048 (order: 1, 16384 bytes)

TCP bind hash table entries: 2048 (order: 0, 8192 bytes)

TCP: Hash tables configured (established 2048 bind 2048)

TCP reno registered

m547x_8x DMA: Initialize Multi-channel DMA API v1.0

JFFS2 version 2.2. (NAND) �© 2001-2006 Red Hat, Inc.

io scheduler noop registered

io scheduler anticipatory registered

io scheduler deadline registered

io scheduler cfq registered (default)

IOIVME Device Driver Registered with MAJOR = 0

Attached IRQ5 vector=69

Attached IRQ6 vector=70

Attached IRQ7 vector=71

Attached IRQ7 vector=71

IOI Device Driver Registered with MAJOR = 0

RESET Device Driver Registered with MAJOR = 0

RTC driver registered with major = 253

DISP DEVICE DRIVER REGISTERED with major = 254

RTS driver registered with major = 248

WDT DEVICE DRIVER REGISTERED with major = 251

req Device Driver Registered with MAJOR = 246

HIMAGNI MEMORY  DEVICE REMAPPED ADDRESS: fc000000

HIMAGNI MEMORY  DEVICE REMAPPED ADDRESS: fb000000

HIMAGNI MEMORY  DEVICE REMAPPED ADDRESS: fc900000

ColdFire internal UART serial driver version 1.00

ttyS0 at 0xf0008600 (irq = 99) is a builtin ColdFire UART

ttyS1 at 0xf0008700 (irq = 98) is a builtin ColdFire UART

ttyS2 at 0xf0008800 (irq = 97) is a builtin ColdFire UART

ttyS3 at 0xf0008900 (irq = 96) is a builtin ColdFire UART

brd: module loaded

loop: module loaded

FEC ENET (DMA) Version 0.20

eth0: ethernet 00:60:72:00:00:01

eth1: ethernet 00:60:72:00:00:02

physmap platform flash device: 007fffff at ff800000

physmap-flash.0: Found 1 x16 devices at 0x0 in 16-bit bank

NOR chip too large to fit in mapping. Attempting to cope...

Amd/Fujitsu Extended Query Table at 0x0040

physmap-flash.0: CFI does not contain boot bank location. Assuming top.

number of CFI chips: 1

cfi_cmdset_0002: Disabling erase-suspend-program due to code brokenness.

Reducing visibility of 8192KiB chip to 8191KiB

2 cmdlinepart partitions found on MTD device physmap-flash.0

Creating 2 MTD partitions on "physmap-flash.0":

0x00000000-0x00280000 : "kernel"

0x00280000-0x007c0000 : "root"

mice: PS/2 mouse device common for all mice

TCP cubic registered

NET: Registered protocol family 1

NET: Registered protocol family 17

NET: Registered protocol family 15

RPC: Registered udp transport module.

RPC: Registered tcp transport module.

VFS: Mounted root (jffs2 filesystem).

inflate returned -3

Unable access at virtual address e304186aps: e3062ecb

PC: [<001090b8>] zlib_inflate+0x738/0x14f0<0>

SR: 2000  SP: 0302da68 a2: 0302a000

d0: 000001ff    d1: 00000000    d2: 00000003    d3: 20000249

d4: 00000000    d5: 00000100    a0: c004452c    a1: c004452c

Process init (pid: 1, stackpage=0302c000)

Stack from 0302da68:

       <0> 00000000<0> 00000003<0> 20000249<0> 00000000<0> 00000100<0> c004452c(0xc004452c)<0> c004452c(0xc004452c)<0> 0302a000

       <0> 000001ff<0> ffffffff<0> 00000000<0> e304186a<0> 00000000<0> 4c0a2000<0> 001090b8<0> 00000000

       <0> 0000001f<0> 00000006<0> 029c4200<0> 03fc4000<0> 0302dbb4<0> 00108980<0> 03041002<0> 000dee9a

       <0> 00001000<0> c004452c(0xc004452c)<0> 00000000<0> 0013e34a<0> 03052814<0> c00442ec(0xc00442ec)<0> 00001000<0> 00fc4000

       <0> 0000c81c<0> c004452c(0xc004452c)<0> c0044068(0xc0044068)<0> c004406c(0xc004406c)<0> c0044050(0xc0044050)<0> c0044054(0xc0044054)          <0> 000001ff<0> c004452c(0xc)

       <0> 0026c81c<0> c004452c(0xc004452c)<0> c00442ec(0xc00442ec)<0> c004452c(0xc004452c)<0> 00002504<0> 029ad000<0> 00000000<0> 00000000

Call Trace:

       <0> [<000e0736>]<0> [<000d16dc>]<0> [<00069660>]<0> [<000d46c0>]

       <0> [<001019e0>]<0> [<0010429e>]<0> [<000d44c0>]<0> [<000d483c>]

       <0> [<00052796>]<0> [<0004a652>]<0> [<000d2e22>]<0> [<000d3156>]

       <0> [<000d3196>]<0> [<00100100>]<0> [<00051d14>]<0> [<00051aac>]

       <0> [<000520e2>]<0> [<00051d50>]<0> [<0004a406>]<0> [<00051d8a>]

       <0> [<0004aee4>]<0> [<00056eb0>]<0> [<0003f398>]<0> [<00058372>]

       <0> [<00058496>]<0> [<001bf48a>]<0> [<001bfd12>]<0> [<0003f398>]

       <0> [<00058372>]<0> [<00022fc6>]<0> [<000251d4>]<0> [<00023952>]

       <0> [<0010453c>]<0> [<00098f40>]<0> [<0009a24e>]<0> [<0003f36c>]

       <0> [<00046a30>]<0> [<0006fdf4>]<0> [<0006fb7a>]<0> [<00070e00>]

       <0> [<00021030>]<0> [<000776c6>]<0> [<000214ae>]<0> [<00048ce2>]

       <0> [<00023a56>]<0> [<0003f36c>]<0> [<00021cc2>]<0> [<0002104c>]

       <0> [<000210a8>]<0> [<00104098>]<0> [<00023998>]<0> [<00021330>]

Kernel panic - not syncing: Attempted to kill init!

标记 (3)
0 项奖励
回复
1 回复

1,883 次查看
marek_neuzil
NXP Employee
NXP Employee

Hello,

Issue has been already reported, see the discussion threadi have bug during booting process it shows jffs2 dies with inflate returned -3

Best Regards,

Marek Neuzil

0 项奖励
回复