imx8mp install ros2 fail

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx8mp install ros2 fail

ソリューションへジャンプ
2,434件の閲覧回数
_距离你
Contributor I

yocto: https://source.codeaurora.org/external/imx/imx-manifest -b imx-linux-zeus -m imx-5.4.70-2.3.0.xml

ros:https://gitee.com/zxd2021-imx/meta-robot-platform/tree/v0.2-L5.4.70-2.3.0/

https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX-%E6%9C%BA%E5%99%A8%E4%BA%BA%E5%B9%B...

I refer to this tutorial to create a ROS development environment. When I configure and compile the ROS2 dashing version, the final compilation generates complete firmware normally. However, I will report an error when compiling ROS2-foxyerror.pngerror.png

The following changes have been made in meta-robot-platform/imx/meta-ros/meta-ros2/recipes-devtools/foonathan-memory/foonathan-memory_git.bb, and compilation errors may also occur

SRCREV_FORMAT = "main"
SRCREV_main = "8f6a027d473f9b4796509158962d8ddf89fbe086"
SRCREV_master = "cf13bff238397aab0d8c49b7f6263233cf8a2396"
SRC_URI = "git://github.com/foonathan/memory.git;protocol=https;name=main \
    git://github.com/foonathan/compatibility.git;protocol=https;name=master;destsuffix=git/cmake/master \
    file://catch-upstream.tgz \
"
Finally, I uploaded the error log file
0 件の賞賛
返信
1 解決策
2,410件の閲覧回数
Harvey021
NXP TechSupport
NXP TechSupport

Hi @_距离你 

Based on the error message, it seems the current revision not available from source uri for the BSP you are using. 

Suggest trying to download the packages manually or change to other BSP.

 

Best regards

Harvey

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,411件の閲覧回数
Harvey021
NXP TechSupport
NXP TechSupport

Hi @_距离你 

Based on the error message, it seems the current revision not available from source uri for the BSP you are using. 

Suggest trying to download the packages manually or change to other BSP.

 

Best regards

Harvey

0 件の賞賛
返信