imx8mp install ros2 fail

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx8mp install ros2 fail

Jump to solution
2,570 Views
_距离你
Contributor I

yocto: https://source.codeaurora.org/external/imx/imx-manifest -b imx-linux-zeus -m imx-5.4.70-2.3.0.xml

ros:https://gitee.com/zxd2021-imx/meta-robot-platform/tree/v0.2-L5.4.70-2.3.0/

https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX-%E6%9C%BA%E5%99%A8%E4%BA%BA%E5%B9%B...

I refer to this tutorial to create a ROS development environment. When I configure and compile the ROS2 dashing version, the final compilation generates complete firmware normally. However, I will report an error when compiling ROS2-foxyerror.png

The following changes have been made in meta-robot-platform/imx/meta-ros/meta-ros2/recipes-devtools/foonathan-memory/foonathan-memory_git.bb, and compilation errors may also occur

SRCREV_FORMAT = "main"
SRCREV_main = "8f6a027d473f9b4796509158962d8ddf89fbe086"
SRCREV_master = "cf13bff238397aab0d8c49b7f6263233cf8a2396"
SRC_URI = "git://github.com/foonathan/memory.git;protocol=https;name=main \
    git://github.com/foonathan/compatibility.git;protocol=https;name=master;destsuffix=git/cmake/master \
    file://catch-upstream.tgz \
"
Finally, I uploaded the error log file
0 Kudos
Reply
1 Solution
2,546 Views
Harvey021
NXP TechSupport
NXP TechSupport

Hi @_距离你 

Based on the error message, it seems the current revision not available from source uri for the BSP you are using. 

Suggest trying to download the packages manually or change to other BSP.

 

Best regards

Harvey

View solution in original post

0 Kudos
Reply
1 Reply
2,547 Views
Harvey021
NXP TechSupport
NXP TechSupport

Hi @_距离你 

Based on the error message, it seems the current revision not available from source uri for the BSP you are using. 

Suggest trying to download the packages manually or change to other BSP.

 

Best regards

Harvey

0 Kudos
Reply