imx8mp install ros2 fail

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

imx8mp install ros2 fail

跳至解决方案
1,563 次查看
_距离你
Contributor I

yocto: https://source.codeaurora.org/external/imx/imx-manifest -b imx-linux-zeus -m imx-5.4.70-2.3.0.xml

ros:https://gitee.com/zxd2021-imx/meta-robot-platform/tree/v0.2-L5.4.70-2.3.0/

https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX-%E6%9C%BA%E5%99%A8%E4%BA%BA%E5%B9%B...

I refer to this tutorial to create a ROS development environment. When I configure and compile the ROS2 dashing version, the final compilation generates complete firmware normally. However, I will report an error when compiling ROS2-foxyerror.png

The following changes have been made in meta-robot-platform/imx/meta-ros/meta-ros2/recipes-devtools/foonathan-memory/foonathan-memory_git.bb, and compilation errors may also occur

SRCREV_FORMAT = "main"
SRCREV_main = "8f6a027d473f9b4796509158962d8ddf89fbe086"
SRCREV_master = "cf13bff238397aab0d8c49b7f6263233cf8a2396"
SRC_URI = "git://github.com/foonathan/memory.git;protocol=https;name=main \
    git://github.com/foonathan/compatibility.git;protocol=https;name=master;destsuffix=git/cmake/master \
    file://catch-upstream.tgz \
"
Finally, I uploaded the error log file
0 项奖励
回复
1 解答
1,539 次查看
Harvey021
NXP TechSupport
NXP TechSupport

Hi @_距离你 

Based on the error message, it seems the current revision not available from source uri for the BSP you are using. 

Suggest trying to download the packages manually or change to other BSP.

 

Best regards

Harvey

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,540 次查看
Harvey021
NXP TechSupport
NXP TechSupport

Hi @_距离你 

Based on the error message, it seems the current revision not available from source uri for the BSP you are using. 

Suggest trying to download the packages manually or change to other BSP.

 

Best regards

Harvey

0 项奖励
回复