configure GPIO as input in imx8mp

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

configure GPIO as input in imx8mp

3,179件の閲覧回数
DEEPIKA19
Contributor I

Hi team

I would like to use the GPIO5_IO25 as a input pin in our design. By default when exported from sysfs I am getting the following value.

 

root@root:/sys/class/gpio/gpio153# cat direction

in

root@root:/sys/class/gpio/gpio153# cat value

0

 

The GPIO5_IO05 is connected to a 10k pullup but the value is 0. Please could someone suggest me on how to debug this. Should any dts changes be added for this?

 

Regards,

Deepika

0 件の賞賛
返信
5 返答(返信)

3,161件の閲覧回数
Dhruvit
NXP TechSupport
NXP TechSupport

Hi @DEEPIKA19,

In the case of the GPIO5_IO25, it should be mentioned that when a GPIO is exported in the sysfs, by default, the direction of the GPIO is set as "input," and the value is set to "zero." The processor itself drives the voltage level of that particular GPIO.

 

For the GPIO5_IO05, please confirm the voltage at the processor side of the GPIO5_IO05 before and after exporting the GPIO. 

And also, please confirm if the GPIO5_IO05 is not used in the device tree by any other peripheral.

 

Thanks & Regards,
Dhruvit.

0 件の賞賛
返信

3,117件の閲覧回数
DEEPIKA19
Contributor I

hi @Dhruvit ,

Thanks for your reply.

 

Regards,

Deepika

0 件の賞賛
返信

3,069件の閲覧回数
Dhruvit
NXP TechSupport
NXP TechSupport

Hi @DEEPIKA19 

If this issue is resolved, then Can I mark this case to close state?

Thanks & Regards

Dhruvit Vasavda

0 件の賞賛
返信

3,059件の閲覧回数
DEEPIKA19
Contributor I

hi @Dhruvit ,

The issue is not resolved.

I tried to add device_init_wakeup(&client->dev, 1) as suggested but i am still facing the the same issue.

Regards,

Deepika

0 件の賞賛
返信

3,038件の閲覧回数
DEEPIKA19
Contributor I

Thanks for your support @Dhruvit ,

The issues is resolved making driver change in reference with similar touch drivers .

 

Regards,

Deepika

0 件の賞賛
返信