compatibility issues for beans codewarrior classic and the version 10

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

compatibility issues for beans codewarrior classic and the version 10

跳至解决方案
3,533 次查看
solucionesvendi
Contributor I

Hi, my problem is that compatibility issues in my program for the beans of LCD that appear in this site

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=PROCESSOR-EXPERT&fpsp=1&tab=Design_To...

 

that beans for example, user interface, ect. How can upgrade my firmware with this beans to v10 of codewarrior?? thanks, best regards

0 项奖励
回复
1 解答
3,313 次查看
ProcessorExpert
Senior Contributor III

Hello,

 

please note that LCD component is not the same as TLCD free component. LCD component is delivered within CW installation but TLCD is additional free sw component. However it seems that this issue was already solved within this post:

 

https://community.freescale.com/message/79700#79700

 

best regards
Vojtech Filip
Processor Expert Support Team

在原帖中查看解决方案

0 项奖励
回复
3 回复数
3,313 次查看
ProcessorExpert
Senior Contributor III

Hello,

 

could you please specify what family of MCUs are you targeting? Generally the Eclipse version of CodeWarrior provides the same set of components as CodeWarrior Classic, so you should be able to use the LCD component (formerly called bean) in the same way as in the Classic version.

 

In case you have some CodeWarriopr Classic project you can use "Classic Importer feature" from eclipse version of CW to import such project or use steps from this https://community.freescale.com/message/91224#91224

 

Could you please also specify what compatibility issue do you mean exactly, because I see any LCD component under your link.

 

Note: The LCD component is from category advanced and you need to have purchased "Professional Suite" to use it or you can buy it separately in PE´s component store.

 

For FSL licensing policy please see this link

 

best regards
Vojtech Filip
Processor Expert Support Team

0 项奖励
回复
3,313 次查看
solucionesvendi
Contributor I

In the link appear a pack of beans, for example, in the package called user interface, appear this beans

this bean is for control a lcd hd44780, when I try to import this bean to v10 codewarrior, give me error, how could import this beans, best regards, is for hcs08 microcontroller, and the version of codewarrior is classic 3.09 processor expert

0 项奖励
回复
3,314 次查看
ProcessorExpert
Senior Contributor III

Hello,

 

please note that LCD component is not the same as TLCD free component. LCD component is delivered within CW installation but TLCD is additional free sw component. However it seems that this issue was already solved within this post:

 

https://community.freescale.com/message/79700#79700

 

best regards
Vojtech Filip
Processor Expert Support Team

0 项奖励
回复