Kinetis K60 ADC0 and ADC1 using same reference VREFH and VREFL

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Kinetis K60 ADC0 and ADC1 using same reference VREFH and VREFL

Jump to solution
3,424 Views
MarkP_
Contributor V

Hi,

PE doesn't allow to select same reference VREFH&VREFL to ADC0 and ADC1.

Is there any reason for this, cannot find in datasheet any restriction.

~Mark

 

Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
2,858 Views
ProcessorExpert
Senior Contributor III

Hello,

 

it is necessary to allow pin sharing to enable selection of VREFH&VREFL pins in both ADC components. You can swicth on this feature using "Pin Sharing" menu command from selected pin´s pop-up menu. For more details please see enclosed screen-shot.

 

For more details about pin sharing please see CW´s help:

CodeWarrior for Microcontrollers V10.x > Processor Expert Manuals > Processor Expert Users Manual > Application Design > Configuring Components > Pin Sharing

 

best regards
Vojtech Filip
Processor Expert Support Team

View solution in original post

0 Kudos
Reply
2 Replies
2,859 Views
ProcessorExpert
Senior Contributor III

Hello,

 

it is necessary to allow pin sharing to enable selection of VREFH&VREFL pins in both ADC components. You can swicth on this feature using "Pin Sharing" menu command from selected pin´s pop-up menu. For more details please see enclosed screen-shot.

 

For more details about pin sharing please see CW´s help:

CodeWarrior for Microcontrollers V10.x > Processor Expert Manuals > Processor Expert Users Manual > Application Design > Configuring Components > Pin Sharing

 

best regards
Vojtech Filip
Processor Expert Support Team

0 Kudos
Reply
2,858 Views
MarkP_
Contributor V

Thank's,

~Mark

0 Kudos
Reply