change signal name

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

change signal name

2,325 Views
gionny
Contributor II

Hi everyone,

I'm using S32 Design Studio with Processor Expert.

Component "PinSettings" really useful.

In GPIO tab I can configure every uP pin.

My problem is this: Can I attach a name to the PIN. In my code I need to use it with a specific name and not with port name / pin number

Thanks

G. Ferrari

Labels (1)
0 Kudos
Reply
3 Replies

2,157 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

HI G Ferrari

You can rename component by right click on the component, choose "Rename Component"

pastedImage_1.png


Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,157 Views
gionny
Contributor II

Thanks for the answer.

I'd like to change single PIN name.

For example:

PTB.2 --> CHIP_RESET

PTE.5 --> CHIP_ENABLE

Is't possible?

Thanks

Gionatha

0 Kudos
Reply

2,157 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

I don't think Component "PinSettings"  has this feature.

Jennie Zhang.

0 Kudos
Reply