about "code for component has not been generate yet"

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

about "code for component has not been generate yet"

Jump to solution
2,661 Views
LiKe
Contributor I

I use MQX3.8 add AD follow <<CW for Microcotrollers v10.x and MQX>> page 139. but I check AD and view source code.

the cw10.x POP "code for component has not been generate yet",why? bye the way, I use windows 7

Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
2,451 Views
ProcessorExpert
Senior Contributor III

Hi,

Could you please write more details on what CodeWarrior version are you using?

 

The Processor Expert code can be generated using the project pop-up menu command "Generate Processor Expert code" or you can use the icon (see attachment) in Processor Expert project panel. Processor Expert project panel can be opened using the command Window > Show view > Other... , select Processor Expert / Project panel.

 

best regards
Petr Hradsky
Processor Expert Support Team

 

 

 

View solution in original post

0 Kudos
Reply
1 Reply
2,452 Views
ProcessorExpert
Senior Contributor III

Hi,

Could you please write more details on what CodeWarrior version are you using?

 

The Processor Expert code can be generated using the project pop-up menu command "Generate Processor Expert code" or you can use the icon (see attachment) in Processor Expert project panel. Processor Expert project panel can be opened using the command Window > Show view > Other... , select Processor Expert / Project panel.

 

best regards
Petr Hradsky
Processor Expert Support Team

 

 

 

0 Kudos
Reply