XIP stops running after boot on custom MIMXRT1015 board

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

XIP stops running after boot on custom MIMXRT1015 board

827件の閲覧回数
EricBuschCDI
Contributor I

Hi, I have a custom board running just a blink example. The board is based on the MIMXRT1015 EVK. It has the same flash chip, but uses the 4A package instead of 5A. Whenever I flash the chip, I can see the flash being programmed on an oscilloscope. The link I am using says it verifies the flash correctly. 

Whenever the MCU boots, I can see the flash start up but immediately stops. Debugging never gets to main. When I execute the code from RAM it works correctly. Has anyone seen something like this?

0 件の賞賛
返信
0 返答(返信)