how to config sja1105 for ls1046afrwy

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

how to config sja1105 for ls1046afrwy

Jump to solution
2,798 Views
fenghua_jiang
Contributor IV

I have a ls1046afrwy board,and sjtag1105s is connect to tms570.

I modify the board ,sjtag1105s connect cpu armv7 by spi;so I need spi drive code.

linux kernel is v5.4.3rt

1.mcu SPI_BASE =0,SPI_EXT =0

2.fsl-ls1046a-frwy.dts

&dspi {
bus-num = <0>;
status = "okay";

sja1105: ethernet-switch@2 {
reg = <0x2>;
#address-cells = <1>;
#size-cells = <0>;
compatible = "nxp,sja1105s";
/* 12 MHz */
spi-max-frequency = <12000000>;
/* Sample data on trailing clock edge */
spi-cpha;
/* SPI controller settings for SJA1105 timing requirements */
fsl,spi-cs-sck-delay = <100>;
fsl,spi-sck-cs-delay = <100>;
};
};

error:

sja1105 spi0.2: Expected device ID 0xae00030e but read 0xffffffff,which means that the switch is not connected to the appropriate SPI Slave Select line.

config :

dspi: spi@2100000 {
compatible = "fsl,ls1021a-v1.0-dspi";
#address-cells = <1>;
#size-cells = <0>;
reg = <0x0 0x2100000 0x0 0x10000>;
interrupts = <GIC_SPI 64 IRQ_TYPE_LEVEL_HIGH>;
clock-names = "dspi";
clocks = <&clockgen 4 1>;
spi-num-chipselects = <4>;
big-endian;
status = "disabled";
};

spi-fsl-dspi.c probe dspi dev,sja1105 sck is right, pcs is right,and sint can see data;

where is the fault?

I donot know that the switch is not connected to the appropriate SPI Slave Select line.

 

 

 

 

Tags (1)
0 Kudos
Reply
1 Solution
2,763 Views
fenghua_jiang
Contributor IV

The problem is resolved.

View solution in original post

0 Kudos
Reply
2 Replies
2,764 Views
fenghua_jiang
Contributor IV

The problem is resolved.

0 Kudos
Reply
2,075 Views
amol_kulkarni1
Contributor II

I am also having similar issue, what was your solution?

 

0 Kudos
Reply