Where is J26 connector on FRDM-K64Z schematics?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Where is J26 connector on FRDM-K64Z schematics?

ソリューションへジャンプ
1,716件の閲覧回数
shauldorf
Contributor V

Where is J26
connector on FRDM-K64Z schematics drawing? I only found Micro USB

On KSDK1.2 component fsl_gpio it exist as you can see from my screen capture

MicroUSB.jpg

K64F_KSDK+PE.jpg

1 解決策
1,479件の閲覧回数
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello shaul dorf:

I think the developers overlooked this for FRDM-K64F. The header is now labeled J4.

I reported this already, but in the meantime the fix is easy. Just open the PinSettings component and go to the Pins view mode. Then you can filter by J26 and change the User Pin/Signal Name:

pastedImage_3.png

Also, there are a couple changes between FRDM-K64F schematics Rev C -> Rev D -> Rev E, according to the board errata of the next link:

http://http//cache.freescale.com/files/32bit/doc/errata/FRDMK64F_ERRATA.pdf

So please check the label at the back of your board and make sure you have the right schematics. According to the version you will need to adjust a couple more pin names, as next:

Rev C:

- No changes apart from J4 label.

Rev D:

- PTC10/PTC11 in header J4 are swapped.

- PTE24/PTE25 in header J2 are swapped.

Rev E:

- Changes in Rev D.

- PTB20 is connected to J6_3 and also to J4_9.

- PTC12 is connected to J2_2.

- PTA0 is NOT connected to J2_2, only to J11_1.

I am sorry for this inconvenience. Let me know if you have questions.

Regards!

Jorge Gonzalez

元の投稿で解決策を見る

2 返答(返信)
1,480件の閲覧回数
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello shaul dorf:

I think the developers overlooked this for FRDM-K64F. The header is now labeled J4.

I reported this already, but in the meantime the fix is easy. Just open the PinSettings component and go to the Pins view mode. Then you can filter by J26 and change the User Pin/Signal Name:

pastedImage_3.png

Also, there are a couple changes between FRDM-K64F schematics Rev C -> Rev D -> Rev E, according to the board errata of the next link:

http://http//cache.freescale.com/files/32bit/doc/errata/FRDMK64F_ERRATA.pdf

So please check the label at the back of your board and make sure you have the right schematics. According to the version you will need to adjust a couple more pin names, as next:

Rev C:

- No changes apart from J4 label.

Rev D:

- PTC10/PTC11 in header J4 are swapped.

- PTE24/PTE25 in header J2 are swapped.

Rev E:

- Changes in Rev D.

- PTB20 is connected to J6_3 and also to J4_9.

- PTC12 is connected to J2_2.

- PTA0 is NOT connected to J2_2, only to J11_1.

I am sorry for this inconvenience. Let me know if you have questions.

Regards!

Jorge Gonzalez

1,479件の閲覧回数
shauldorf
Contributor V

Jorge Thanks;

As usual, fast and correct answer.

By the way I have an open half answer question posted on Jul. 2.

The question relates to” I/O with Host via OpenSDA”.

The discussion is located on Kinetis Design Studio and not in Kinetis Software Development Kit may be this is the reason.

The first part related to KL25Z has been answered by Erich, but the all issues pointed to K64F are still open.

B.R

Shaul

0 件の賞賛
返信