Use procesor expert default problem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Use procesor expert default problem

Jump to solution
3,376 Views
marceladueñas
Contributor II

Hello everybody, i try to update to kds 3.2 and sdk 2.0 , a terrible idea because now all my projects have the next issue: 
ERROR: at line 1: {{DEVELOPMENT}} The symbol "UseProcessorExpertDefault" was used without testing %ifdef or %if defined(). It's recommended to use %get() instead (if possible). (file: Beans\CriticalSection\CriticalSection.chg) V3 CS1 Processor Expert Problem

i try to comeback again , i uninstall all and comeback to the 3.0 version but the issue is the same , an even if i choose freRtos or procesor expert there is an error . I don't know what more can i do. HELP!!!

Labels (1)
1 Solution
3,160 Views
BlackNight
NXP Employee
NXP Employee

Hi Marcela,

make sure you have this setting disabled:

pastedImage_1.png

I hope this helps,

Erich

View solution in original post

2 Replies
3,161 Views
BlackNight
NXP Employee
NXP Employee

Hi Marcela,

make sure you have this setting disabled:

pastedImage_1.png

I hope this helps,

Erich

3,160 Views
marceladueñas
Contributor II

You are so brilliant!!, it solve all the errors and warnings.

Thank you so much.

Regards

0 Kudos
Reply