Unknown error with key StandardEditionMCU 11.0, LM_BADSYSDATE

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Unknown error with key StandardEditionMCU 11.0, LM_BADSYSDATE

1,936 Views
MWMinor
Contributor V

Hi, I have recently purchased a new licence for my Codewarrior software. I had been using V10.6.4 but after generating the license and placing it in the correct /MCU directory, when I started Codewarrior, I received an "unknown error....." message as above.

I have installed V11.0 of the tool but the error is the same.

Can anyone please help...?

0 Kudos
Reply
3 Replies

1,752 Views
MWMinor
Contributor V

Hi Erich

I can't see the text "System clock has been set back" anywhere.

I did have an issue when booting my PC a couple of weeks ago whereby the system clock was modified to a date in 2020..!!!

Codewarrior wasn't running at the time.

I put the clock right and re-booted my machine.

I then searched for any files dated out to 2020 and deleted them.

Maybe I missed something..????

Thanks again for your support.

ken

0 Kudos
Reply

1,752 Views
BlackNight
NXP Employee
NXP Employee

Hi Ken,

ok, I'll get in touch with you directly to close the loop.

Erich

0 Kudos
Reply

1,752 Views
BlackNight
NXP Employee
NXP Employee

Does it say as well "System clock has been set back."?

This is in general an indication that somehow the date of the system has been set back (or in other words: there are files with 'future' time/date present on your system.

Did you change the system time/date?

0 Kudos
Reply