Setting loopback request in PCIe training sequence via T2080 RC

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Setting loopback request in PCIe training sequence via T2080 RC

1,280 Views
scottgerhold
Contributor IV

I am trying to use Serdes Val to test a link that has a switch on the other end. The switch can be configured to go into a loopback mode if the T2080 were to set the loopback bit in the TS1 sequence. Can the tool be used to push the external EP into that mode? Is there anything in the T2080 register space that I can configure via SW or an emulator to set that bit in the training sequence?

0 Kudos
Reply
0 Replies