USB HS Processor Expert

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

USB HS Processor Expert

ソリューションへジャンプ
1,786件の閲覧回数
sam_
Contributor III

We are trying to use the USBHS for the K65 in Processor Expert.  When we add a component, it indicates that only USB full-speed is supported.  When will the high-speed support be added?

pastedImage_0.png

ラベル(1)
0 件の賞賛
返信
1 解決策
1,515件の閲覧回数
marek_neuzil
NXP Employee
NXP Employee

Hello,

The USBHS device should be supported in the next release of Kinetis SDK 1.3.0 (Processor Expert Kinetis SDK Support - Eclipse update package).

Best Regards,

Marek Neuzil

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,515件の閲覧回数
marek_neuzil
NXP Employee
NXP Employee

Hello,

The USBHS device should be supported in the next release of Kinetis SDK 1.3.0 (Processor Expert Kinetis SDK Support - Eclipse update package).

Best Regards,

Marek Neuzil

0 件の賞賛
返信