Track instruction causing Check machine issue

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Track instruction causing Check machine issue

3,960 次查看
Nadiatova
Contributor I

I have a machne check issue with programm on MPC5674F​.

After a primary investigation and register values evaluation and referring to the map file and the reference manual, it's a write bus error occured due to memcpy instruction trying to write in a reserved area of the memory.

Since memcpy is wide used in the program I want to track which function called the memcpy function to know the Data/pointer causing the error? Is there any other registers I can read or Is there a specific other way using maybe map and hex file?

I hope I get a helpful answer from you. Thanks in advance.

0 项奖励
回复
3 回复数

3,914 次查看
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi @Nadiatova 

which debugger do you have? You can check Call Stack. If you have S32 Design Studio, take a look at a screenshot in this thread:

https://community.nxp.com/t5/S32-Design-Studio/where-to-see-function-call-stack/td-p/754999

If you use Trace32, then select View -> Stackframe.

This should help to find where it comes from.

Regards,

Lukas

0 项奖励
回复

3,908 次查看
Nadiatova
Contributor I

Hi,

thanks for your reply. I'm using greenhills! the issue is once it's debugging mode the machine check exeption is never. What I'm doing to read registers is to save them in signals which I can read via Canape.

I there any registers I can read to get the call stack?

0 项奖励
回复

3,884 次查看
lukaszadrapa
NXP TechSupport
NXP TechSupport

It's not about reading of registers, it would be necessary to analyze the stack. You can take a look at "3.2.2. The Stack Frame" in attached document.

Another option is to use tracing tools if you have Nexus connector on the board or use some kind of SW method.

Regards,

Lukas

0 项奖励
回复