Timer Unit bean and ticks

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Timer Unit bean and ticks

Jump to solution
2,730 Views
Jeinstei
Contributor II

Hi-

I noticed that in CW 10.3, the TimerUnit bean doesn't support ticks anymore. Is there something I am missing? For using external clocks, not having ticks makes the bean almost impossible to use if the clock input is something like a motor or fan counter. Should I be using a different bean?

Thanks,

Josh E

Tags (2)
0 Kudos
Reply
1 Solution
2,447 Views
Petr_H
NXP Employee
NXP Employee

Hi,

I suppose you mean the settings of "offset" or "Period" values of the channel.

The timer ticks unit are supported only if the counter frequency is not set to "Auto select".

You have to specify the Counter frequency to some valid value (if you don't know, type there current value from third column) and then the timer-ticks unit appear in the list of possible units and it can be used.

best regards

Petr Hradsky

Processor Expert Support Team

View solution in original post

0 Kudos
Reply
2 Replies
2,448 Views
Petr_H
NXP Employee
NXP Employee

Hi,

I suppose you mean the settings of "offset" or "Period" values of the channel.

The timer ticks unit are supported only if the counter frequency is not set to "Auto select".

You have to specify the Counter frequency to some valid value (if you don't know, type there current value from third column) and then the timer-ticks unit appear in the list of possible units and it can be used.

best regards

Petr Hradsky

Processor Expert Support Team

0 Kudos
Reply
2,447 Views
Jeinstei
Contributor II

Thanks Petr. That looks to have done the trick for what I'm doing!

0 Kudos
Reply