Timer Unit bean and ticks

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Timer Unit bean and ticks

ソリューションへジャンプ
2,797件の閲覧回数
Jeinstei
Contributor II

Hi-

I noticed that in CW 10.3, the TimerUnit bean doesn't support ticks anymore. Is there something I am missing? For using external clocks, not having ticks makes the bean almost impossible to use if the clock input is something like a motor or fan counter. Should I be using a different bean?

Thanks,

Josh E

ラベル(2)
タグ(2)
0 件の賞賛
返信
1 解決策
2,514件の閲覧回数
Petr_H
NXP Employee
NXP Employee

Hi,

I suppose you mean the settings of "offset" or "Period" values of the channel.

The timer ticks unit are supported only if the counter frequency is not set to "Auto select".

You have to specify the Counter frequency to some valid value (if you don't know, type there current value from third column) and then the timer-ticks unit appear in the list of possible units and it can be used.

best regards

Petr Hradsky

Processor Expert Support Team

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,514件の閲覧回数
Petr_H
NXP Employee
NXP Employee

Hi,

I suppose you mean the settings of "offset" or "Period" values of the channel.

The timer ticks unit are supported only if the counter frequency is not set to "Auto select".

You have to specify the Counter frequency to some valid value (if you don't know, type there current value from third column) and then the timer-ticks unit appear in the list of possible units and it can be used.

best regards

Petr Hradsky

Processor Expert Support Team

0 件の賞賛
返信
2,514件の閲覧回数
Jeinstei
Contributor II

Thanks Petr. That looks to have done the trick for what I'm doing!

0 件の賞賛
返信