T1042 high resolution timer support

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

T1042 high resolution timer support

4,522 次查看
dshtaingus
Contributor I

Hi All,

Our customer asking if a T1042 is supporting high resolution timer in Linux.

He wants to set it to 1000 Hz.

I didn't found any information regarding this issue.

I can configure option " CONFIG_HIGH_RES_TIMERS" in kernel, but according to help text:

" This option enables high resolution timer support. If your hardware is not capable then this option only increases the size of the kernel image."

Someone can help with this issue?

Thanks in advace

标记 (1)
0 项奖励
回复
5 回复数

4,416 次查看
yipingwang
NXP TechSupport
NXP TechSupport

Please configure 

HZ_1000=y

CONFIG_HIGH_RES_TIMERS=y

0 项奖励
回复

4,416 次查看
dshtaingus
Contributor I

Good day,

Thanks for the answer.

But I would like to know if there is a HW support?

To configure two fields in .config it's cool, but according to the comment, there must to be a HW support.

So my question is still remained: "Does T1042 has HW support in high resolution timer?"

Regards

0 项奖励
回复

4,416 次查看
yipingwang
NXP TechSupport
NXP TechSupport

 "CONFIG_HIGH_RES_TIMERS=y" was enabled for for PowerPC RT kernels in SDK release.

You may go ahead and try the config option.

0 项奖励
回复

4,416 次查看
dshtaingus
Contributor I

Good day,

Is there any news regarding my question?

Regards

0 项奖励
回复

4,416 次查看
dshtaingus
Contributor I

Hey,

As I mentioned before, my task was to ensure our customer, that T1042 is supporting high resolution timer in Linux.

I don't need to compile nothing for now.

I just need to find some kind of official documentation, in which there would be clearly explained that issue.

The modification and compilation of kernel are future task.

Meanwhile we are in "go / no go" situation.

Can you point me or provide the information I'm looking for?

I tried to look for that info, but without success so far.

Regards

0 项奖励
回复