We want to use ATF05MS003N(or ATF05MS006N), MHT1803A, MMRF1310HSR5 in our product at 40.68 MHz.
The datasheet reference circuit gives Zsource and Zload values for frequencies from 135-174 and 350-520 MHz.
The S parameter file covers 240-1000 MHz.
A similar question mentioned the AFT05MS003N_PDK file, which no longer exists.
Could you help to provide(ATF05MS003N/ATF05MS006N/MHT1803A/MMRF1310HSR5) reference circuit/S para/PDK at 40.68MHz?
Datasheet provides impedance values measured on real boards. We have no measured data to share for frequencies not covered by available reference circuits.
Impedance characterization is a special task that requires time and resources. Generally, we perform impedance characterization for circuits which are included into the device datasheets. We have many other designs which have not been tested to measure impedances.
Using ADS models is the recommended way to design an amplifier. Model design kits for most devices are available on the device product pages.
Please, you can create a ticket to technical support for a specific device. We will do our best to help you.
Have a great day,
Pavel
TIC
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------