SJA1110 SDL Non Secure Image

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SJA1110 SDL Non Secure Image

3,074件の閲覧回数
Jeba
Contributor I

Hi, I am trying trying to send firmware to SJA1110 using SPI. The used modus modus operandi is SDL Non Secure Mode . SJA1110  is responding correctly , it transits the State from INITIALIZING to WAITING, but it is not moving to the state VALIDATING_IMG_META_DATA. Do I need to provide any bytes before the marker 0xA66AA66AA66AA66A? e.g Stream Header, Operation Byte? If so , what should be these bytes

 

Thank you

0 件の賞賛
返信
1 返信

3,048件の閲覧回数
PavelL
NXP Employee
NXP Employee

Hello @Jeba ,

this information can be shared only under NDA. The information has been lost in the latest version Rev 2.0 of UM11107. Please download the previous version Rev 1.1.

Best regards,

Pavel

0 件の賞賛
返信