SJA1110 SDL Non Secure Image

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SJA1110 SDL Non Secure Image

3,118 Views
Jeba
Contributor I

Hi, I am trying trying to send firmware to SJA1110 using SPI. The used modus modus operandi is SDL Non Secure Mode . SJA1110  is responding correctly , it transits the State from INITIALIZING to WAITING, but it is not moving to the state VALIDATING_IMG_META_DATA. Do I need to provide any bytes before the marker 0xA66AA66AA66AA66A? e.g Stream Header, Operation Byte? If so , what should be these bytes

 

Thank you

0 Kudos
Reply
1 Reply

3,092 Views
PavelL
NXP Employee
NXP Employee

Hello @Jeba ,

this information can be shared only under NDA. The information has been lost in the latest version Rev 2.0 of UM11107. Please download the previous version Rev 1.1.

Best regards,

Pavel

0 Kudos
Reply