SDHC PE Component in MQX 4.0 issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SDHC PE Component in MQX 4.0 issue

1,057 Views
sushantamohanra
Contributor I

Hi All,

I am using Processor Expert in CW 10.4 in an MQX 4.0 project to store and read raw bytes from a SDHC card using the SDHC_LDD module.

I face the following issue, when I execute the MQX project containing the PE defined SDHC_LDD module the code freezes at SetBusClockPrescalers. But when I execute the same code in a standalone PE generated project with no MQX the initialization is fine.

Can someone please point out what I am missing here. Please let me know what details will be required about my project and I will gladly furnish them.

Thanks and with best regards,

Sushanta.

Tags (4)
0 Kudos
Reply
0 Replies