Processor Expert sets wrong clock mode for K02FN64

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Processor Expert sets wrong clock mode for K02FN64

1,319件の閲覧回数
scottm
Senior Contributor II

I'm using PEx with KSDK 1.3 on one project (yeah, I know, I'm working on moving off of it) and I discovered that it's not setting the MCG BLPE mode correctly.  If you choose BLPE in a clock configuration, it comes out as kMcgModePBE - which doesn't exist on this part.  The result is that when you try to switch to it, it looks up the appropriate transition from its matrix and gets the wrong answer, so it's perpetually stuck transitioning to FEI mode.

Here's a screenshot:

Screenshot 2017-11-25 17.01.37.png

My fix for now is to disable the 'read only' option for the structure that it generates and override the setting myself:

clkLowPower.mcgConfig.mcg_mode = kMcgModeBLPE;

The clock manager is such a large chunk of code that I'm planning to ditch it as soon as I have time, so I'm not too worried about this but I thought I'd warn anyone else who might come across it.

Scott

タグ(1)
0 件の賞賛
返信
1 返信

1,178件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello ,

Thanks for your sharing.

BR

Alice

0 件の賞賛
返信