Processor Expert command line code generation

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Processor Expert command line code generation

ソリューションへジャンプ
6,091件の閲覧回数
julian15
Contributor I

Does anyone know a way to make Processor Expert (CDE or M. Driver Suite) to trigger code generation from the command line? I would like to automate this for  a build server.

Any help is appreciated.

Thank you!

1 解決策
5,426件の閲覧回数
BlackNight
NXP Employee
NXP Employee
8 返答(返信)
5,426件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Hi Julian,

Currently (up to MCU10.4) this is not supported. I have filed a feature request on this and I epect that the next version should support this. So we need to wait a bit.

I hope this helps.

5,426件の閲覧回数
tchermak
Contributor I

Do we know if this feature made it in for MCU10.5?

0 件の賞賛
返信
5,426件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Hi Tim,

it made it into 10.5. I have documented it here:

Eclipse Command Line Code Generation with Processor Expert | MCU on Eclipse

5,425件の閲覧回数
overdamped
Contributor II

Any word on when they'll be releasing Processor Expert Driver Suite 10.5? This feature is definitely something I could use in my IAR prebuild scripts...

0 件の賞賛
返信
5,426件の閲覧回数
BlackNight
NXP Employee
NXP Employee

There are no definitive release plans for 10.5 available yet.

5,425件の閲覧回数
tchermak
Contributor I

Excellent - thanks!!

0 件の賞賛
返信
5,426件の閲覧回数
BlackNight
NXP Employee
NXP Employee

To my knowledge it did. I need to dig out the details how to use it.

0 件の賞賛
返信
5,426件の閲覧回数
julian15
Contributor I

Thank you for the info Erich!

0 件の賞賛
返信