Processor Expert Vybrid DDR3 Init_DDR TXSNR error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Processor Expert Vybrid DDR3 Init_DDR TXSNR error

ソリューションへジャンプ
1,667件の閲覧回数
McuG
Contributor II

We are trying to initialize the DDR3 module (and to verify our settings) using the Init_DDR module in Processor Expert (Vybrid). All values are filled from the DDR3 datasheet I get an error for the timing configuration , TXSNR field (while it is calculated as per JEDEC 8*txs). Is there a way of bypassing this error and generate the code ? Does anyone know the formula that is used inside PE for validation ?

0 件の賞賛
返信
1 解決策
1,451件の閲覧回数
McuG
Contributor II

Updated to DriverSuite_10.4.3_update.zip , and the problem was addressed (we were using DriverSuite_10.4_Install_into_Eclipse_3.7_4.2.zip initially, not aware of the update).

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,452件の閲覧回数
McuG
Contributor II

Updated to DriverSuite_10.4.3_update.zip , and the problem was addressed (we were using DriverSuite_10.4_Install_into_Eclipse_3.7_4.2.zip initially, not aware of the update).

0 件の賞賛
返信