Processor Expert Support for K26

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Processor Expert Support for K26

1,677 次查看
thomasolenik
Contributor III

Are there any plans to support the K26 in KDS Processor Expert? The availability of PE support is a major factor in MCU selection for me. If I have a project that can be done with an MCU supported by PE, I use it. Not having PE support opens the decision up to other competitive product lines.

标记 (3)
0 项奖励
回复
2 回复数

1,430 次查看
BlackNight
NXP Employee
NXP Employee

Hi Thomas,

if you add the SDK V1.3 from Welcome to Kinetis Expert | Kinetis Expert , then you can create SDK V1.3 Processor Expert projects

pastedImage_1.png

But it is true that there is no Processor Expert any more with the SDK V2.0.

I hope this helps,

Erich

0 项奖励
回复

1,430 次查看
thomasolenik
Contributor III

Interesting. I don't think I've ever selected SDK and PE at the same time. A lot of my projects require CAN and the SDKs are a little weak for CAN bit timing. PE makes it so easy. 

0 项奖励
回复