Kinetis K22 timer components with runtime period selection?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Kinetis K22 timer components with runtime period selection?

1,018件の閲覧回数
scottm
Senior Contributor II

The TimerInt component has methods for setting the timer period at runtime, but I've been unable to find any configuration that will let me do that on a K22.  I can't find any mention in the documentation of what hardware is supported.  For any available timer type, I get 'error in inherited component' and a message that runtime setting isn't available.

Is there such an option for the K22?  I'm using CodeWarrior 10.7 and no, I can't move this project to KDS and KSDK.

If I have to configure the flextimer manually I'll do that, but I hate to bypass PE for something that it's clearly intended to be able to do.

Thanks,

Scott

ラベル(1)
0 件の賞賛
返信
0 返答(返信)