Processor Expert: Kinetis K60 CPU

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Processor Expert: Kinetis K60 CPU

跳至解决方案
3,435 次查看
pende
Contributor III

Hi,

I tried PE for clocking purposes and I found out, that its impossible to reach an allowed FLL reference clock with  TWR-K60512

I can switch between external reference clock 50 MHz and 25 MHz (from TWR-SER).

--> see attachments

 

What's wrong?

Regards, Philip

标签 (1)
标记 (1)
0 项奖励
回复
1 解答
2,768 次查看
ProcessorExpert
Senior Contributor III

Hello,

 

this behavior is correct and I think it corresponds to the PE documentation and the reference manual. In case you need to use the requested values its necessary to switch to the BLPE or PEE mode. Please note that the FLL clock is still running in FBE mode. For more details pleas see K60 reference manual (24.4.1.1 MCG Modes of Operation chapter).

 

best regards
Vojtech Filip
Processor Expert Support Team

在原帖中查看解决方案

0 项奖励
回复
1 回复
2,769 次查看
ProcessorExpert
Senior Contributor III

Hello,

 

this behavior is correct and I think it corresponds to the PE documentation and the reference manual. In case you need to use the requested values its necessary to switch to the BLPE or PEE mode. Please note that the FLL clock is still running in FBE mode. For more details pleas see K60 reference manual (24.4.1.1 MCG Modes of Operation chapter).

 

best regards
Vojtech Filip
Processor Expert Support Team

0 项奖励
回复