Processor Expert: Kinetis K60 CPU

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Processor Expert: Kinetis K60 CPU

Jump to solution
3,450 Views
pende
Contributor III

Hi,

I tried PE for clocking purposes and I found out, that its impossible to reach an allowed FLL reference clock with  TWR-K60512

I can switch between external reference clock 50 MHz and 25 MHz (from TWR-SER).

--> see attachments

 

What's wrong?

Regards, Philip

Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
2,783 Views
ProcessorExpert
Senior Contributor III

Hello,

 

this behavior is correct and I think it corresponds to the PE documentation and the reference manual. In case you need to use the requested values its necessary to switch to the BLPE or PEE mode. Please note that the FLL clock is still running in FBE mode. For more details pleas see K60 reference manual (24.4.1.1 MCG Modes of Operation chapter).

 

best regards
Vojtech Filip
Processor Expert Support Team

View solution in original post

0 Kudos
Reply
1 Reply
2,784 Views
ProcessorExpert
Senior Contributor III

Hello,

 

this behavior is correct and I think it corresponds to the PE documentation and the reference manual. In case you need to use the requested values its necessary to switch to the BLPE or PEE mode. Please note that the FLL clock is still running in FBE mode. For more details pleas see K60 reference manual (24.4.1.1 MCG Modes of Operation chapter).

 

best regards
Vojtech Filip
Processor Expert Support Team

0 Kudos
Reply