Processor Expert: Kinetis K60 CPU

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Processor Expert: Kinetis K60 CPU

ソリューションへジャンプ
3,400件の閲覧回数
pende
Contributor III

Hi,

I tried PE for clocking purposes and I found out, that its impossible to reach an allowed FLL reference clock with  TWR-K60512

I can switch between external reference clock 50 MHz and 25 MHz (from TWR-SER).

--> see attachments

 

What's wrong?

Regards, Philip

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
2,733件の閲覧回数
ProcessorExpert
Senior Contributor III

Hello,

 

this behavior is correct and I think it corresponds to the PE documentation and the reference manual. In case you need to use the requested values its necessary to switch to the BLPE or PEE mode. Please note that the FLL clock is still running in FBE mode. For more details pleas see K60 reference manual (24.4.1.1 MCG Modes of Operation chapter).

 

best regards
Vojtech Filip
Processor Expert Support Team

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,734件の閲覧回数
ProcessorExpert
Senior Contributor III

Hello,

 

this behavior is correct and I think it corresponds to the PE documentation and the reference manual. In case you need to use the requested values its necessary to switch to the BLPE or PEE mode. Please note that the FLL clock is still running in FBE mode. For more details pleas see K60 reference manual (24.4.1.1 MCG Modes of Operation chapter).

 

best regards
Vojtech Filip
Processor Expert Support Team

0 件の賞賛
返信