Problem of Processor Expert generated low power BSP code for K60F for 2 MHz clock configuration

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Problem of Processor Expert generated low power BSP code for K60F for 2 MHz clock configuration

1,264 Views
kirankunnath
Contributor II

Hi,

We are testing low power  mode for K60 Tower board.

Processor Expert generated low power BSP code on for K60F for 2 MHz clock configuration and the VLPR power mode is not working as it is getting stuck in an endless while loop.

while((MCG_S & MCG_S_IRCST_MASK) == 0x00U) { /* Check that the source internal reference clock is fast clock. */

        }

It was mentioned that the CW10.2 version has this problem but it is rectified in CW10.3 version. We are using CW10.5 with MQX 4.0 . but still has this problem.
Kindly provide the solution for resolving the same.

Regards,

Kiran

0 Kudos
Reply
1 Reply

1,126 Views
Petr_H
NXP Employee
NXP Employee

Hi,

I'm sorry, but we are not able to reproduce the problem.

Could you provide us some simple test project showing the issue ?

best regards

Petr Hradsky

Processor Expert Support Team

0 Kudos
Reply