Possible bug in Processor Expert and KDS 3.0?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Possible bug in Processor Expert and KDS 3.0?

跳至解决方案
2,278 次查看
dave408
Senior Contributor II

This is 100% reproducible for me under KDS 3.0.  If I delete the Generated_Code folder and then click "Generate Processor Expert Code" (for example, if I want to clean up a project because I have removed many components), Processor Expert will create the Generated_Code folder and the SDK sub folder and the operation completes, but it will not create the other source files, like Cpu.h, Cpu.cpp, etc.

Anyone else having this problem?  If I delete only the contents of the Generated_Code folder, it usually hangs when I click the generate code button.  If it hangs on the writing files step, after closing KDS, the files referenced above appear.

0 项奖励
回复
1 解答
1,994 次查看
liborukropec
NXP Employee
NXP Employee

Do you delete the Generated_Code folder inside the Eclipse, or outside (other File manager, Explorer, etc)? The latter can confuse Eclipse.\

EDIT: I reproduced the issue when the folder is deleted outside of the eclipse independently on Eclipse preferences for refreshing workspace. I'll log bug report.

Workaround: delete the folder inside the eclipse project explorer.

在原帖中查看解决方案

0 项奖励
回复
6 回复数
1,994 次查看
liborukropec
NXP Employee
NXP Employee

Hello,

can you share more details, what processor, what SDK version are you using and if you use stock KDS 3.0 or whether you installed any update?

Thank you,

Libor

0 项奖励
回复
1,994 次查看
dave408
Senior Contributor II

This happens with the MK64FN1M0VLL12, MK22FN256VLL12, and MK22FN128VLL10, which are the processors we currently use.  I only have installed the required eclipse update for KSDK 1.2 and the MQX TAD plugin.  I am using KSDK 1.2.0.

0 项奖励
回复
1,995 次查看
liborukropec
NXP Employee
NXP Employee

Do you delete the Generated_Code folder inside the Eclipse, or outside (other File manager, Explorer, etc)? The latter can confuse Eclipse.\

EDIT: I reproduced the issue when the folder is deleted outside of the eclipse independently on Eclipse preferences for refreshing workspace. I'll log bug report.

Workaround: delete the folder inside the eclipse project explorer.

0 项奖励
回复
1,994 次查看
dave408
Senior Contributor II

Thanks, Libor.  I do delete it from outside of Eclipse, but I will use your workaround in the future!

0 项奖励
回复
1,994 次查看
MarekTrmac
NXP Employee
NXP Employee

I'd recommend to set both "Refresh" check-boxes located under "Window - Preferences - General - Workspace". This improve detection of changes, that are done on the disk outside the Eclipse.

0 项奖励
回复
1,994 次查看
BlackNight
NXP Employee
NXP Employee

Setting that 'Refresh' option in "Window - Preferences - General - Workspace" generally is not recommended, as it slows down Eclipse.

Instead, doing an F5 (or context menu > Refresh) should help too.

Erich

0 项奖励
回复