PEx error-messages after update KSDK-V1.2 -> V1.3

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PEx error-messages after update KSDK-V1.2 -> V1.3

1,579件の閲覧回数
oaf
Contributor IV

Hi,

KDS-V3.0, Win7, MK66FX1M0VMD18

We had a project running just fine under KSDK-V1.2.

When KSDK-V1.3 arrived we updated (automatic converter) our project, and now we got some peculiar error messages:

Cannot create new item, could not load item: symbol = LinkItem item = Beans\OS_Task\Items\1.3.0\OS_Task_links.item

Cannot create new item, could not load item: symbol = LinkItem item = Beans\OS_Task\Items\1.3.0\OS_Task_links.item

Cannot create new item, could not load item: symbol = LinkItem item = Beans\OS_Task\Items\1.3.0\OS_Task_links.item

Cannot create new item, could not load item: symbol = LinkItem item = Beans\OS_Task\Items\1.3.0\OS_Task_links.item

Cannot create new item, could not load item: symbol = LinkItem item = Beans\OS_Task\Items\1.3.0\OS_Task_links.item

Cannot create new item, could not load item: symbol = LinkItem item = Beans\OS_Task\Items\1.3.0\OS_Task_links.item

Cannot create new item, could not load item: symbol = LinkItem item = Beans\OS_Task\Items\1.3.0\OS_Task_links.item

Cannot create new item, could not load item: symbol = SdkSpecificMethodsMasterInt item = Beans\fsl_dspi\Items\1.3.0\fsl_dspi_master_methods.item

Cannot create new item, could not load item: symbol = SdkSpecificMethodsSlaveInt item = Beans\fsl_dspi\Items\1.3.0\fsl_dspi_slave_methods.item

Cannot create new item, could not load item: symbol = SdkSpecificMethodsMasterDma item = Beans\fsl_dspi\Items\1.3.0\fsl_dspi_masterDma_methods.item

Cannot create new item, could not load item: symbol = SdkSpecificMethodsSlaveDma item = Beans\fsl_dspi\Items\1.3.0\fsl_dspi_slaveDma_methods.item

Cannot create new item, could not load item: symbol = SdkSpecificMethodsMasterInt item = Beans\fsl_dspi\Items\1.3.0\fsl_dspi_master_methods.item

Cannot create new item, could not load item: symbol = SdkSpecificMethodsSlaveInt item = Beans\fsl_dspi\Items\1.3.0\fsl_dspi_slave_methods.item

Cannot create new item, could not load item: symbol = SdkSpecificMethodsMasterDma item = Beans\fsl_dspi\Items\1.3.0\fsl_dspi_masterDma_methods.item

Cannot create new item, could not load item: symbol = SdkSpecificMethodsSlaveDma item = Beans\fsl_dspi\Items\1.3.0\fsl_dspi_slaveDma_methods.item

Cannot create new item, could not load item: symbol = SdkSpecificMethodsMasterInt item = Beans\fsl_dspi\Items\1.3.0\fsl_dspi_master_methods.item

Cannot create new item, could not load item: symbol = SdkSpecificMethodsSlaveInt item = Beans\fsl_dspi\Items\1.3.0\fsl_dspi_slave_methods.item

Cannot create new item, could not load item: symbol = SdkSpecificMethodsMasterDma item = Beans\fsl_dspi\Items\1.3.0\fsl_dspi_masterDma_methods.item

Cannot create new item, could not load item: symbol = SdkSpecificMethodsSlaveDma item = Beans\fsl_dspi\Items\1.3.0\fsl_dspi_slaveDma_methods.item

Please don't tell me to make my project from scratch, as it will take several days!!!

PS:Are the KSDK not intended for use by professionals? We have a lot of problems when update from V1.1 as well, and needless to say this is not a quality we could use for our products if this is the level of quality which is embedded in this development system.

タグ(3)
0 件の賞賛
返信
1 返信

1,430件の閲覧回数
marek_neuzil
NXP Employee
NXP Employee

Hello,

I have discussed the issue with the responsible Processor Expert developer and the conversion of the project should be possible without any issue. Could you provide me the project for analysis, please? (I need the whole project or the ProcessorExpert.pe file from the project at least)

Best Regards,

Marek Neuzil

0 件の賞賛
返信