PWM_LDD or TimerOut_LDD

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PWM_LDD or TimerOut_LDD

2,287件の閲覧回数
haroldvogel
Contributor II

I am new to Processor Expert.  Using Code Warrior 10.6 for MKL36Z128VLL4 and MKL36Z256VLL4.  I am trying to send a 2Khz to 5Khz signal to a Piezoelectric device.  I have tried setting up the TimerOut_LDD but methods SetPulseWidthUS/MS and SetPulseWidth are grayed out, this signal is to be a 50% duty cycle and from reading online documents it seems that the TimerOut_LDD is the way to go.

The TimerOut_LDD refers to a 'Runtime setting" which needs to be configured to have the above items available.  I cannot find this value nor can I find an explanation, that I understand, of what it is or where it is located.

Am I using the right item or should I go with the PWM_LDD or some other way?

For any way that I should go I would like detailed instructions on how to set it up and why this is the way to go.

Thanks in advance for your help.

ラベル(2)
0 件の賞賛
返信
3 返答(返信)

1,867件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

this question was answered

Re: Processor Expert TimerOut_LDD

0 件の賞賛
返信

1,867件の閲覧回数
haroldvogel
Contributor II

Thank you for the information.

I post about using PDD worked great.

John Vogel

0 件の賞賛
返信

1,867件の閲覧回数
haroldvogel
Contributor II

Update.  The signal is to be triggered when a button is pressed so this item is not interrupt driven and I cannot seem to disable that selection other than not having the code generate and event function for this process.

0 件の賞賛
返信