PE components are created but do not show up in CW10

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PE components are created but do not show up in CW10

Jump to solution
2,199 Views
quevedo
Contributor V

Hello,

 

I am moving to CW10, and I am trying to create a new project from scratch for the TWR-MECH board (target processor MCF52259). I want to use Processor Expert (PE). My CodeWarrior is Version 10.1, Build Id 110726, Special Edition. During the "create new project" wizard, I selected the bare target processor, not any of the option for tower boards.

 

I selected a PE component (PWM Component) at the Components Library pane, then I clicked on it with the right button, and selected "Add to project" option. However, the PWM component did not show up at the Project Panel (and I cannot see any "Embedded Components" folder inside the project either). My first thought was that I did not select the Add option correctly, so I tried that again. No changes. The CPU component  also does not show up right after the new project wizard finished, as it happened in previous versions of CW.

 

So I tried to click on the "Generate Processor Expert Project" button at the Project Panel. I get an error message stating that there is some error. Looking at the Problems tab, I find errors related to PWM1 and PWM2 components. When I double-click on one of these messages, the Component Inspector pane is loaded with the config options of the PWM component, showing the errors: unassigned timings for period and starting pulse width. it means that the components were created, but do not show up in the Project Panel.

 

I right-clicked at the project panel and chose Refresh to see what happened. Nothing.

 

I suppose it has something to do with the CW configuration. I can configure any components that are not fully configured when created (because of the errors), but after configured i cannot access them anymore.

 

How can I fix it? Just a reminder, the installation is brand new, I did not alter any default configs. I also tried the same install in 2 computers (one running WinXP and the other on Windows 7).

 

Thanks in advance

0 Kudos
Reply
1 Solution
1,895 Views
quevedo
Contributor V

You are right. I could not find the Embedded Components folder because it is within the "Processor Expert.pe" element. The icon for this looks like a text file, thus I did not notice the "+" sign that allowed me to expand that element. Now I can see all PE components, PWMs and CPU.

 

Thanks!

View solution in original post

0 Kudos
Reply
2 Replies
1,895 Views
ProcessorExpert
Senior Contributor III

Hello,

 

It seems you have overlooked “Embedded Component” folder on the project panel. You should unfold this folder to show all components in the project. I have also tried to add the PWM component to the M52559 PE project in CW V10.1 (B110726) and I have not encountered any problem.

 

Below, you can find steps how to properly add a new component to the project in eclipse:

 

  1. Make a focus on the project where you want add a component (e.g. click on the CPU component).
  2. Go to the “Components Library” and add a component by double clicking on it or using appropriate menu command from selected component´s pop-menu.
  3. Unfold Embedded Components folder.

 

For more details please see enclosed scren-shot.

 

best regards
Vojtech Filip
Processor Expert Support Team

0 Kudos
Reply
1,896 Views
quevedo
Contributor V

You are right. I could not find the Embedded Components folder because it is within the "Processor Expert.pe" element. The icon for this looks like a text file, thus I did not notice the "+" sign that allowed me to expand that element. Now I can see all PE components, PWMs and CPU.

 

Thanks!

0 Kudos
Reply