NFS boot of LS1088ardb

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

NFS boot of LS1088ardb

ソリューションへジャンプ
4,184件の閲覧回数
LeonP
Contributor II

I will be very glad for your help in the following:

I extracted the FIT image in QSPI of my LS1088ARDB as a file into my PC.
I disassembled it into components: DTB, Kernel, INITRD.
Than I load all three into RAM similar to Management Complex does and do "booti...".
Everything runs fine except:
- when original system boots I see the lines like:
 fsl_mc_allocator dpmcp.18: Adding to iommu group 6
- but when "my" boot occurs these lines are absent, but no errors appear even when I add "debug ignore_loglevel earlyprintk printk.devkmsg=on" to bootargs.
To be on the safe side - my "bootargs" is the same as original, except that I added initrd location (which isn't important as the difference is in the kernel boot, before FS).
Obviously, "my" booted kernel also doesn't work with DPMACx saying there is no such devices.

I can't imagine what may be the cause of such difference, if kernel and device tree are exactly the same in both cases.

タグ(2)
0 件の賞賛
返信
1 解決策
4,133件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Please download dpl file to  0x80d00000, then execute the following command before boot Linux.

=>fsl_mc lazyapply dpl 0x80d00000

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
4,134件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Please download dpl file to  0x80d00000, then execute the following command before boot Linux.

=>fsl_mc lazyapply dpl 0x80d00000

0 件の賞賛
返信
4,007件の閲覧回数
LeonP
Contributor II

Thank you, yipingwang.

Your advice really worked for some time.

I don't know what i did incorrect but starting from Monday I can't boot into NFS again.
Everything looks fine but wireshark shows no packets from the board.
Here is the log file:

<14:12:52.824> NOTICE: UDIMM 18ADF2G72AZ-2G6E1

<14:12:54.487> NOTICE: 16 GB DDR4, 64-bit, CL=15, ECC on, CS0+CS1
<14:12:54.487> NOTICE: BL2: v2.8(release):lf-6.1.55-2.2.0-0-g08e9d4eef-dirty
<14:12:54.488> NOTICE: BL2: Built : 17:05:34, Mar 12 2024
<14:12:55.256> NOTICE: BL2: Booting BL31
<14:12:55.273> NOTICE: BL31: v2.8(release):lf-6.1.55-2.2.0-0-g08e9d4eef-dirty
<14:12:55.273> NOTICE: BL31: Built : 17:05:34, Mar 12 2024
<14:12:55.279> NOTICE: Welcome to ls1088ardb BL31 Phase


<14:12:55.317> U-Boot 2023.04 (Mar 11 2024 - 15:32:53 +0200)

<14:12:55.317> SoC: LS1088AE Rev1.0 (0x87030010)
<14:12:55.358> Clock Configuration:
<14:12:55.358> CPU0(A53):1600 MHz CPU1(A53):1600 MHz CPU2(A53):1600 MHz
<14:12:55.367> CPU3(A53):1600 MHz CPU4(A53):1600 MHz CPU5(A53):1600 MHz
<14:12:55.370> CPU6(A53):1600 MHz CPU7(A53):1600 MHz
<14:12:55.370> Bus: 700 MHz DDR: 2100 MT/s
<14:12:55.373> Reset Configuration Word (RCW):
<14:12:55.373> 00000000: 4000541c 00000040 00000000 00000000
<14:12:55.375> 00000010: 00000000 000a0000 00300000 00000000
<14:12:55.377> 00000020: 030011a0 00002580 00000000 00000040
<14:12:55.377> 00000030: 0000005b 00000000 00002403 00000000
<14:12:55.379> 00000040: 00000000 00000000 00000000 00000000
<14:12:55.380> 00000050: 00000000 00000000 00000000 00000000
<14:12:55.380> 00000060: 00000000 00000000 00000011 000009e7
<14:12:55.381> 00000070: 44110000 00107777
<14:12:55.381> VID: Core voltage after adjustment is at 1000 mV
<14:12:55.382> DRAM: 15.9 GiB
<14:12:55.382> DDR 15.9 GiB (DDR4, 64-bit, CL=15, ECC on)
<14:12:55.383> DDR Chip-Select Interleaving Mode: CS0+CS1
<14:12:55.415> Using SERDES1 Protocol: 29 (0x1d)
<14:12:55.415> Using SERDES2 Protocol: 19 (0x13)
<14:12:55.415> PCIe1: pcie@3400000 Root Complex: no link
<14:12:55.416> PCIe2: pcie@3500000 disabled
<14:12:55.416> PCIe3: pcie@3600000 Root Complex: no link
<14:12:55.417> Core: 61 devices, 22 uclasses, devicetree: separate
<14:12:55.419> NAND: 512 MiB
<14:12:55.419> MMC: FSL_SDHC: 0
<14:12:55.419> Loading Environment from SPIFlash... SF: Detected s25fs512s with page size 256 Bytes, erase size 256 KiB, total 64 MiB
<14:12:55.451> *** Warning - bad CRC, using default environment

<14:12:55.451> EEPROM: NXID v1
<14:12:55.482> In: serial
<14:12:55.482> Out: serial
<14:12:55.482> Err: serial
<14:12:55.482> Model: NXP Layerscape 1088a RDB Board
<14:12:55.484> Board: LS1088ARDB-PB, Board Arch: V1, Board version: B, boot from QSPI:1
<14:12:55.485> CPLD: v5.0
<14:12:55.485> SERDES1 Reference : Clock1 = 100MHz Clock2 = 156.25MHz
<14:12:55.515> SERDES2 Reference : Clock1 = 100MHz Clock2 = 100MHz
<14:12:55.519> Net: eth0: DPMAC1@xgmii [PRIME]PHY reset timed out
<14:12:56.073> , eth1: DPMAC2@xgmii, eth2: DPMAC3@qsgmii, eth3: DPMAC4@qsgmii, eth4: DPMAC5@qsgmii, eth5: DPMAC6@qsgmii, eth6: DPMAC7@qsgmii, eth7
: DPMAC8@qsgmii, eth8: DPMAC9@qsgmii, eth9: DPMAC10@qsgmii
<14:12:56.621> SF: Detected s25fs512s with page size 256 Bytes, erase size 256 KiB, total 64 MiB
<14:12:56.706> device 0 offset 0xa00000, size 0x200000
<14:12:58.342> SF: 2097152 bytes @ 0xa00000 Read: OK
<14:12:58.342> device 0 offset 0xe00000, size 0x100000
<14:12:59.171> SF: 1048576 bytes @ 0xe00000 Read: OK
<14:13:00.052> crc32+ MC firmware version 10.10.0

<14:13:00.083> fsl-mc: Booting Management Complex ... SUCCESS
<14:13:00.415> fsl-mc: Management Complex booted (version: 10.10.0, boot status: 0x1)
<14:13:00.485> Hit any key to stop autoboot: 0
<14:13:00.518> =>
<14:13:12.159> => sf read 0x80001000 0xd00000 0x100000;run mcinitcmd;fsl_mc lazyapply dpl 0x80001000;
<14:13:14.916> device 0 offset 0xd00000, size 0x100000
<14:13:15.767> SF: 1048576 bytes @ 0xd00000 Read: OK
<14:13:15.770> SF: Detected s25fs512s with page size 256 Bytes, erase size 256 KiB, total 64 MiB
<14:13:15.785> device 0 offset 0xa00000, size 0x200000
<14:13:17.473> SF: 2097152 bytes @ 0xa00000 Read: OK
<14:13:17.479> device 0 offset 0xe00000, size 0x100000
<14:13:18.329> SF: 1048576 bytes @ 0xe00000 Read: OK
<14:13:18.342> fsl-mc: MC is already booted
<14:13:18.342> => set MyK 0xa0000000; set MyKc 0xB0000000; set MyD 0xAF000000;
<14:13:20.452> => set ethact eth4; set ipaddr 192.168.1.1; set serverip 192.168.1.57;
<14:13:22.738> => set kernel_comp_addr_r ${MyKc}; set kernel_comp_size 15185058
<14:13:24.775> => tftpboot ${MyK} fsl.bin
<14:13:25.651> Using DPMAC5@qsgmii device
<14:13:25.651> TFTP from server 192.168.1.57; our IP address is 192.168.1.1
<14:13:25.666> Filename 'fsl.bin'.
<14:13:25.666> Load address: 0xa0000000
<14:13:25.666> Loading: #################################################################
<14:13:25.758> #################################################################
<14:13:25.850> #################################################################
<14:13:25.941> #################################################################
<14:13:26.002> #################################################################
<14:13:26.094> #################################################################
<14:13:26.157> #################################################################
<14:13:26.251> #################################################################
<14:13:26.313> #################################################################
<14:13:26.405> #################################################################
<14:13:26.468> #################################################################
<14:13:26.560> #################################################################
<14:13:26.622> #################################################################
<14:13:26.713> #################################################################
<14:13:26.774> #################################################################
<14:13:26.869> ############################################################
<14:13:26.930> 11.5 MiB/s
<14:13:26.930> done
<14:13:26.930> Bytes transferred = 15185058 (e7b4a2 hex)
<14:13:26.943> => tftpboot ${MyD} fsl.dtb
<14:13:27.341> Using DPMAC5@qsgmii device
<14:13:27.341> TFTP from server 192.168.1.57; our IP address is 192.168.1.1
<14:13:27.393> Filename 'fsl.dtb'.
<14:13:27.393> Load address: 0xaf000000
<14:13:27.393> Loading: ##
<14:13:27.399> 2.4 MiB/s
<14:13:27.399> done
<14:13:27.399> Bytes transferred = 25505 (63a1 hex)
<14:13:27.399> => set kernel_comp_addr_r ${MyKc}
<14:13:28.038> => set kernel_comp_size 15185058
<14:13:28.541> => set bootargs 'console=ttyS0,115200 earlycon=uart8250,mmio,0x21c0500 ramdisk_size=0x3000000 default_hugepagesz=2m hugepagesz=2m h
ugepages=256 ip=192.168.1.1:192.168.1.57:192.168.1.1:255.255.255.0::eth0:off rootdelay=1 root=/dev/nfs rw noinitrd nfsroot=192.168.1.57:/opt/LS108
8/FS_LS1088,vers=3,proto=tcp,nolock'
<14:13:33.681> => booti ${MyK} - ${MyD}
<14:13:34.139> Uncompressing Kernel Image
<14:13:34.541> ## Flattened Device Tree blob at af000000
<14:13:34.599> Booting using the fdt blob at 0xaf000000
<14:13:34.626> Working FDT set to af000000
<14:13:34.626> Loading Device Tree to 000000009fff6000, end 000000009ffff3a0 ... OK
<14:13:34.630> Working FDT set to 9fff6000
<14:13:34.630> WARNING: fdt_fixup_stdout: could not read serial0 alias: FDT_ERR_NOTFOUND
<14:13:34.631> fsl-mc: Deploying data path layout ... SUCCESS

<14:13:34.819> Starting kernel ...

<14:13:34.819> [ 0.000000] Booting Linux on physical CPU 0x0000000000 [0x410fd034]
<14:13:34.845> [ 0.000000] Linux version 5.10.35 (jenkins@pluto) (aarch64-linux-gnu-gcc (Ubuntu 9.3.0-17ubuntu1~20.04) 9.3.0, GNU ld (GNU Binut
ils for Ubuntu) 2.34) #1 SMP PREEMPT Fri Aug 27 22:03:58 CST 2021
<14:13:34.857> [ 0.000000] Machine model: LS1088ARDB-PB Board
<14:13:34.860> [ 0.000000] earlycon: uart8250 at MMIO 0x00000000021c0500 (options '')
<14:13:34.863> [ 0.000000] printk: bootconsole [uart8250] enabled
<14:13:34.864> [ 0.000000] efi: UEFI not found.
<14:13:34.864> [ 0.000000] cma: Reserved 32 MiB at 0x00000000f9c00000
<14:13:35.000> [ 0.000000] NUMA: No NUMA configuration found
<14:13:35.080> [ 0.000000] NUMA: Faking a node at [mem 0x0000000080000000-0x000000837fffffff]
<14:13:35.141> [ 0.000000] NUMA: NODE_DATA [mem 0x837e2fab00-0x837e2fcfff]
<14:13:35.154> [ 0.000000] Zone ranges:
<14:13:35.154> [ 0.000000] DMA [mem 0x0000000080000000-0x00000000ffffffff]
<14:13:35.157> [ 0.000000] DMA32 empty
<14:13:35.159> [ 0.000000] Normal [mem 0x0000000100000000-0x000000837fffffff]
<14:13:35.161> [ 0.000000] Movable zone start for each node
<14:13:35.161> [ 0.000000] Early memory node ranges
<14:13:35.168> [ 0.000000] node 0: [mem 0x0000000080000000-0x00000000fbdfffff]
<14:13:35.171> [ 0.000000] node 0: [mem 0x0000008080000000-0x000000837fffffff]
<14:13:35.171> [ 0.000000] Initmem setup node 0 [mem 0x0000000080000000-0x000000837fffffff]
<14:13:35.173> [ 0.000000] psci: probing for conduit method from DT.
<14:13:35.175> [ 0.000000] psci: PSCIv1.1 detected in firmware.
<14:13:35.177> [ 0.000000] psci: Using standard PSCI v0.2 function IDs
<14:13:35.179> [ 0.000000] psci: MIGRATE_INFO_TYPE not supported.
<14:13:35.179> [ 0.000000] psci: SMC Calling Convention v1.2
<14:13:35.180> [ 0.000000] percpu: Embedded 24 pages/cpu s60120 r8192 d29992 u98304
<14:13:35.181> [ 0.000000] Detected VIPT I-cache on CPU0
<14:13:35.181> [ 0.000000] CPU features: detected: ARM erratum 845719
<14:13:35.184> [ 0.000000] CPU features: detected: GIC system register CPU interface
<14:13:35.187> [ 0.000000] CPU features: kernel page table isolation forced ON by KASLR
<14:13:35.189> [ 0.000000] CPU features: detected: Kernel page table isolation (KPTI)
<14:13:35.191> [ 0.000000] Built 1 zonelists, mobility grouping on. Total pages: 3595776
<14:13:35.192> [ 0.000000] Policy zone: Normal
<14:13:35.192> [ 0.000000] Kernel command line: console=ttyS0,115200 earlycon=uart8250,mmio,0x21c0500 ramdisk_size=0x3000000 default_hugepagesz
=2m hugepagesz=2m hugepages=256 ip=192.168.1.1:192.168.1.57:192.168.1.1:255.255.255.0::eth0:off rootdelay=1 root=/dev/nfs rw noinitrd nfsroot=192.
168.1.57:/opt/LS1088/FS_LS1088,vers=3,proto=tcp,nolock
<14:13:35.271> [ 0.000000] Dentry cache hash table entries: 2097152 (order: 12, 16777216 bytes, linear)
<14:13:35.280> [ 0.000000] Inode-cache hash table entries: 1048576 (order: 11, 8388608 bytes, linear)
<14:13:35.284> [ 0.000000] mem auto-init: stack:off, heap alloc:off, heap free:off
<14:13:35.286> [ 0.000000] software IO TLB: mapped [mem 0x00000000f5c00000-0x00000000f9c00000] (64MB)
<14:13:35.379> [ 0.000000] Memory: 14188024K/14612480K available (20416K kernel code, 3074K rwdata, 9944K rodata, 6656K init, 1035K bss, 391688
K reserved, 32768K cma-reserved)
<14:13:35.524> [ 0.000000] rcu: Preemptible hierarchical RCU implementation.
<14:13:35.524> [ 0.000000] rcu: RCU event tracing is enabled.
<14:13:35.533> [ 0.000000] rcu: RCU restricting CPUs from NR_CPUS=16 to nr_cpu_ids=8.
<14:13:35.536> [ 0.000000] Trampoline variant of Tasks RCU enabled.
<14:13:35.537> [ 0.000000] rcu: RCU calculated value of scheduler-enlistment delay is 25 jiffies.
<14:13:35.539> [ 0.000000] rcu: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=8
<14:13:35.541> [ 0.000000] NR_IRQS: 64, nr_irqs: 64, preallocated irqs: 0
<14:13:35.544> [ 0.000000] GICv3: GIC: Using split EOI/Deactivate mode
<14:13:35.544> [ 0.000000] GICv3: 256 SPIs implemented
<14:13:35.546> [ 0.000000] GICv3: 0 Extended SPIs implemented
<14:13:35.546> [ 0.000000] GICv3: Distributor has no Range Selector support
<14:13:35.547> [ 0.000000] GICv3: 16 PPIs implemented
<14:13:35.549> [ 0.000000] GICv3: CPU0: found redistributor 0 region 0:0x0000000006100000
<14:13:35.550> [ 0.000000] ITS [mem 0x06020000-0x0603ffff]
<14:13:35.550> [ 0.000000] ITS@0x0000000006020000: allocated 65536 Devices @8080080000 (flat, esz 8, psz 64K, shr 0)
<14:13:35.560> [ 0.000000] ITS: using cache flushing for cmd queue
<14:13:35.560> [ 0.000000] GICv3: Using preallocated redistributor tables
<14:13:35.563> [ 0.000000] GICv3: using LPI property table @0x000000837ff00000
<14:13:35.569> [ 0.000000] GICv3: CPU0: using reserved LPI pending table @0x000000837ff10000
<14:13:35.571> [ 0.000000] random: get_random_bytes called from start_kernel+0x32c/0x4f0 with crng_init=0
<14:13:35.572> [ 0.000000] arch_timer: cp15 timer(s) running at 25.00MHz (phys).
<14:13:35.576> [ 0.000000] clocksource: arch_sys_counter: mask: 0xffffffffffffff max_cycles: 0x5c409fb33, max_idle_ns: 440795203156 ns
<14:13:35.580> [ 0.000003] sched_clock: 56 bits at 25MHz, resolution 39ns, wraps every 4398046511103ns
<14:13:35.581> [ 0.008687] Console: colour dummy device 80x25
<14:13:35.584> [ 0.013222] Calibrating delay loop (skipped), value calculated using timer frequency.. 50.00 BogoMIPS (lpj=100000)
<14:13:35.586> [ 0.023670] pid_max: default: 32768 minimum: 301
<14:13:35.588> [ 0.028408] LSM: Security Framework initializing
<14:13:35.588> [ 0.033168] Mount-cache hash table entries: 32768 (order: 6, 262144 bytes, linear)
<14:13:35.589> [ 0.040842] Mountpoint-cache hash table entries: 32768 (order: 6, 262144 bytes, linear)
<14:13:35.593> [ 0.049854] rcu: Hierarchical SRCU implementation.
<14:13:35.593> [ 0.054801] Platform MSI: gic-its@6020000 domain created
<14:13:35.595> [ 0.060217] PCI/MSI: /interrupt-controller@6000000/gic-its@6020000 domain created
<14:13:35.627> [ 0.067811] fsl-mc MSI: gic-its@6020000 domain created
<14:13:35.650> [ 0.073805] EFI services will not be available.
<14:13:35.652> [ 0.078568] smp: Bringing up secondary CPUs ...
<14:13:35.652> [ 0.083457] Detected VIPT I-cache on CPU1
<14:13:35.653> [ 0.083476] GICv3: CPU1: found redistributor 1 region 0:0x0000000006120000
<14:13:35.656> [ 0.083490] GICv3: CPU1: using reserved LPI pending table @0x000000837ff20000
<14:13:35.658> [ 0.083513] CPU1: Booted secondary processor 0x0000000001 [0x410fd034]
<14:13:35.659> [ 0.083839] Detected VIPT I-cache on CPU2
<14:13:35.659> [ 0.083851] GICv3: CPU2: found redistributor 2 region 0:0x0000000006140000
<14:13:35.661> [ 0.083861] GICv3: CPU2: using reserved LPI pending table @0x000000837ff30000
<14:13:35.663> [ 0.083880] CPU2: Booted secondary processor 0x0000000002 [0x410fd034]
<14:13:35.694> [ 0.084196] Detected VIPT I-cache on CPU3
<14:13:35.722> [ 0.084209] GICv3: CPU3: found redistributor 3 region 0:0x0000000006160000
<14:13:35.724> [ 0.084219] GICv3: CPU3: using reserved LPI pending table @0x000000837ff40000
<14:13:35.726> [ 0.084237] CPU3: Booted secondary processor 0x0000000003 [0x410fd034]
<14:13:35.728> [ 0.084561] Detected VIPT I-cache on CPU4
<14:13:35.730> [ 0.084581] GICv3: CPU4: found redistributor 100 region 0:0x0000000006180000
<14:13:35.731> [ 0.084596] GICv3: CPU4: using reserved LPI pending table @0x000000837ff50000
<14:13:35.734> [ 0.084625] CPU4: Booted secondary processor 0x0000000100 [0x410fd034]
<14:13:35.736> [ 0.084979] Detected VIPT I-cache on CPU5
<14:13:35.736> [ 0.084993] GICv3: CPU5: found redistributor 101 region 0:0x00000000061a0000
<14:13:35.738> [ 0.085004] GICv3: CPU5: using reserved LPI pending table @0x000000837ff60000
<14:13:35.739> [ 0.085023] CPU5: Booted secondary processor 0x0000000101 [0x410fd034]
<14:13:35.771> [ 0.085355] Detected VIPT I-cache on CPU6
<14:13:35.785> [ 0.085370] GICv3: CPU6: found redistributor 102 region 0:0x00000000061c0000
<14:13:35.787> [ 0.085381] GICv3: CPU6: using reserved LPI pending table @0x000000837ff70000
<14:13:35.789> [ 0.085400] CPU6: Booted secondary processor 0x0000000102 [0x410fd034]
<14:13:35.791> [ 0.085725] Detected VIPT I-cache on CPU7
<14:13:35.791> [ 0.085741] GICv3: CPU7: found redistributor 103 region 0:0x00000000061e0000
<14:13:35.793> [ 0.085752] GICv3: CPU7: using reserved LPI pending table @0x000000837ff80000
<14:13:35.795> [ 0.085771] CPU7: Booted secondary processor 0x0000000103 [0x410fd034]
<14:13:35.796> [ 0.085827] smp: Brought up 1 node, 8 CPUs
<14:13:35.828> [ 0.263886] SMP: Total of 8 processors activated.
<14:13:35.828> [ 0.268632] CPU features: detected: 32-bit EL0 Support
<14:13:35.835> [ 0.273826] CPU features: detected: CRC32 instructions
<14:13:35.836> [ 0.279011] CPU features: detected: 32-bit EL1 Support
<14:13:35.836> [ 0.292830] CPU: All CPU(s) started at EL2
<14:13:35.836> [ 0.296984] alternatives: patching kernel code
<14:13:35.840> [ 0.302616] devtmpfs: initialized
<14:13:35.873> [ 0.309204] KASLR enabled
<14:13:35.873> [ 0.311955] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 7645041785100000 ns
<14:13:35.893> [ 0.321792] futex hash table entries: 2048 (order: 5, 131072 bytes, linear)
<14:13:35.895> [ 0.329596] pinctrl core: initialized pinctrl subsystem
<14:13:35.895> [ 0.335577] DMI not present or invalid.
<14:13:35.899> [ 0.339778] NET: Registered protocol family 16
<14:13:35.899> [ 0.345498] DMA: preallocated 2048 KiB GFP_KERNEL pool for atomic allocations
<14:13:35.902> [ 0.353109] DMA: preallocated 2048 KiB GFP_KERNEL|GFP_DMA pool for atomic allocations
<14:13:35.904> [ 0.361629] DMA: preallocated 2048 KiB GFP_KERNEL|GFP_DMA32 pool for atomic allocations
<14:13:35.908> [ 0.369728] audit: initializing netlink subsys (disabled)
<14:13:35.938> [ 0.375289] audit: type=2000 audit(0.244:1): state=initialized audit_enabled=0 res=1
<14:13:35.943> [ 0.375887] thermal_sys: Registered thermal governor 'step_wise'
<14:13:35.943> [ 0.383108] thermal_sys: Registered thermal governor 'power_allocator'
<14:13:35.950> [ 0.389439] cpuidle: using governor menu
<14:13:35.950> [ 0.400392] hw-breakpoint: found 6 breakpoint and 4 watchpoint registers.
<14:13:35.953> [ 0.407336] ASID allocator initialised with 32768 entries
<14:13:35.955> [ 0.413622] Serial: AMBA PL011 UART driver
<14:13:35.955> [ 0.417820] imx mu driver is registered.
<14:13:35.958> [ 0.421799] imx rpmsg driver is registered.
<14:13:35.989> [ 0.437453] Machine: LS1088ARDB-PB Board
<14:13:35.989> [ 0.441410] SoC family: QorIQ LS1088A
<14:13:35.999> [ 0.445096] SoC ID: svr:0x87030010, Revision: 1.0
<14:13:35.999> [ 0.453431] fsl_mc_bus 80c000000.fsl-mc: MC firmware version: 10.10.0
<14:13:36.000> [ 0.462493] fsl_mc_dprc dprc.1: DMA mask not set
<14:13:36.034> [ 0.482299] HugeTLB registered 2.00 MiB page size, pre-allocated 256 pages
<14:13:36.034> [ 0.489345] HugeTLB registered 1.00 GiB page size, pre-allocated 0 pages
<14:13:36.060> [ 0.496106] HugeTLB registered 32.0 MiB page size, pre-allocated 0 pages
<14:13:36.061> [ 0.502866] HugeTLB registered 64.0 KiB page size, pre-allocated 0 pages
<14:13:36.063> [ 0.510847] cryptd: max_cpu_qlen set to 1000
<14:13:36.125> [ 0.581320] raid6: neonx8 gen() 2868 MB/s
<14:13:36.222> [ 0.653369] raid6: neonx8 xor() 2138 MB/s
<14:13:36.285> [ 0.725415] raid6: neonx4 gen() 2915 MB/s
<14:13:36.373> [ 0.797465] raid6: neonx4 xor() 2121 MB/s
<14:13:36.434> [ 0.869515] raid6: neonx2 gen() 2793 MB/s
<14:13:36.559> [ 0.941565] raid6: neonx2 xor() 1971 MB/s
<14:13:36.559> [ 1.013623] raid6: neonx1 gen() 2431 MB/s
<14:13:36.625> [ 1.085666] raid6: neonx1 xor() 1663 MB/s
<14:13:36.699> [ 1.157721] raid6: int64x8 gen() 1988 MB/s
<14:13:36.766> [ 1.229759] raid6: int64x8 xor() 1046 MB/s
<14:13:36.841> [ 1.301801] raid6: int64x4 gen() 2217 MB/s
<14:13:36.909> [ 1.373845] raid6: int64x4 xor() 1110 MB/s
<14:13:37.028> [ 1.445897] raid6: int64x2 gen() 1890 MB/s
<14:13:37.060> [ 1.517938] raid6: int64x2 xor() 974 MB/s
<14:13:37.140> [ 1.589979] raid6: int64x1 gen() 1398 MB/s
<14:13:37.247> [ 1.662024] raid6: int64x1 xor() 746 MB/s
<14:13:37.247> [ 1.666328] raid6: using algorithm neonx4 gen() 2915 MB/s
<14:13:37.250> [ 1.671770] raid6: .... xor() 2121 MB/s, rmw enabled
<14:13:37.254> [ 1.676776] raid6: using neon recovery algorithm
<14:13:37.254> [ 1.681796] ACPI: Interpreter disabled.
<14:13:37.255> [ 1.686527] iommu: Default domain type: Passthrough
<14:13:37.257> [ 1.691661] vgaarb: loaded
<14:13:37.257> [ 1.694580] SCSI subsystem initialized
<14:13:37.257> [ 1.698579] usbcore: registered new interface driver usbfs
<14:13:37.258> [ 1.704135] usbcore: registered new interface driver hub
<14:13:37.258> [ 1.709510] usbcore: registered new device driver usb
<14:13:37.263> [ 1.714911] imx-i2c 2000000.i2c: can't get pinctrl, bus recovery not supported
<14:13:37.264> [ 1.722379] i2c i2c-0: IMX I2C adapter registered
<14:13:37.264> [ 1.727462] mc: Linux media interface: v0.10
<14:13:37.272> [ 1.731783] videodev: Linux video capture interface: v2.00
<14:13:37.274> [ 1.737374] pps_core: LinuxPPS API ver. 1 registered
<14:13:37.305> [ 1.742389] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <[email protected]>
<14:13:37.312> [ 1.751609] PTP clock support registered
<14:13:37.313> [ 1.755632] EDAC MC: Ver: 3.0.0
<14:13:37.313> [ 1.759439] No BMan portals available!
<14:13:37.316> [ 1.763381] QMan: Allocated lookup table at (____ptrval____), entry count 65537
<14:13:37.319> [ 1.770854] No QMan portals available!
<14:13:37.319> [ 1.774779] No USDPAA memory, no 'fsl,usdpaa-mem' in device-tree
<14:13:37.320> [ 1.781074] fsl-ifc 2240000.ifc: Freescale Integrated Flash Controller
<14:13:37.322> [ 1.787678] fsl-ifc 2240000.ifc: IFC version 2.0, 8 banks
<14:13:37.328> [ 1.793237] FPGA manager framework
<14:13:37.361> [ 1.796717] Advanced Linux Sound Architecture Driver Initialized.
<14:13:37.361> [ 1.803840] clocksource: Switched to clocksource arch_sys_counter
<14:13:37.368> [ 1.810130] VFS: Disk quotas dquot_6.6.0
<14:13:37.371> [ 1.814126] VFS: Dquot-cache hash table entries: 512 (order 0, 4096 bytes)
<14:13:37.373> [ 1.821183] pnp: PnP ACPI: disabled
<14:13:37.373> [ 1.828806] NET: Registered protocol family 2
<14:13:37.375> [ 1.833534] tcp_listen_portaddr_hash hash table entries: 8192 (order: 5, 131072 bytes, linear)
<14:13:37.377> [ 1.842364] TCP established hash table entries: 131072 (order: 8, 1048576 bytes, linear)
<14:13:37.410> [ 1.851122] TCP bind hash table entries: 65536 (order: 8, 1048576 bytes, linear)
<14:13:37.432> [ 1.859166] TCP: Hash tables configured (established 131072 bind 65536)
<14:13:37.435> [ 1.865923] UDP hash table entries: 8192 (order: 6, 262144 bytes, linear)
<14:13:37.437> [ 1.872974] UDP-Lite hash table entries: 8192 (order: 6, 262144 bytes, linear)
<14:13:37.439> [ 1.880558] NET: Registered protocol family 1
<14:13:37.441> [ 1.885192] RPC: Registered named UNIX socket transport module.
<14:13:37.442> [ 1.891170] RPC: Registered udp transport module.
<14:13:37.442> [ 1.895922] RPC: Registered tcp transport module.
<14:13:37.445> [ 1.900667] RPC: Registered tcp NFSv4.1 backchannel transport module.
<14:13:37.446> [ 1.907167] PCI: CLS 0 bytes, default 64
<14:13:37.447> [ 1.912026] hw perfevents: enabled with armv8_cortex_a53 PMU driver, 7 counters available
<14:13:37.505> [ 1.920470] kvm [1]: IPA Size Limit: 40 bits
<14:13:37.505> [ 1.925898] kvm [1]: vgic-v2@c0e0000
<14:13:37.508> [ 1.929514] kvm [1]: GIC system register CPU interface enabled
<14:13:37.508> [ 1.935502] kvm [1]: vgic interrupt IRQ9
<14:13:37.511> [ 1.939597] kvm [1]: Hyp mode initialized successfully
<14:13:37.512> [ 1.947242] Initialise system trusted keyrings
<14:13:37.512> [ 1.951806] workingset: timestamp_bits=42 max_order=22 bucket_order=0
<14:13:37.512> [ 1.958724] squashfs: version 4.0 (2009/01/31) Phillip Lougher
<14:13:37.515> [ 1.964785] NFS: Registering the id_resolver key type
<14:13:37.517> [ 1.969891] Key type id_resolver registered
<14:13:37.517> [ 1.974109] Key type id_legacy registered
<14:13:37.518> [ 1.978168] nfs4filelayout_init: NFSv4 File Layout Driver Registering...
<14:13:37.524> [ 1.984930] nfs4flexfilelayout_init: NFSv4 Flexfile Layout Driver Registering...
<14:13:37.556> [ 1.992405] jffs2: version 2.2. (NAND) © 2001-2006 Red Hat, Inc.
<14:13:37.556> [ 1.998690] fuse: init (API version 7.32)
<14:13:37.563> [ 2.002836] 9p: Installing v9fs 9p2000 file system support
<14:13:37.594> [ 2.035610] xor: measuring software checksum speed
<14:13:37.594> [ 2.043468] 8regs : 3255 MB/sec
<14:13:37.620> [ 2.050491] 32regs : 3738 MB/sec
<14:13:37.620> [ 2.057997] arm64_neon : 3163 MB/sec
<14:13:37.624> [ 2.062388] xor: using function: 32regs (3738 MB/sec)
<14:13:37.625> [ 2.067483] Key type asymmetric registered
<14:13:37.625> [ 2.071612] Asymmetric key parser 'x509' registered
<14:13:37.626> [ 2.076547] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 243)
<14:13:37.629> [ 2.084071] io scheduler mq-deadline registered
<14:13:37.630> [ 2.088646] io scheduler kyber registered
<14:13:37.661> [ 2.098500] layerscape-pcie 3400000.pcie: host bridge /soc/pcie@3400000 ranges:
<14:13:37.690> [ 2.105894] layerscape-pcie 3400000.pcie: IO 0x2000010000..0x200001ffff -> 0x0000000000
<14:13:37.695> [ 2.114507] layerscape-pcie 3400000.pcie: MEM 0x2040000000..0x207fffffff -> 0x0040000000
<14:13:37.696> [ 2.123218] layerscape-pcie 3400000.pcie: PCI host bridge to bus 0000:00
<14:13:37.699> [ 2.129983] pci_bus 0000:00: root bus resource [bus 00-ff]
<14:13:37.701> [ 2.135517] pci_bus 0000:00: root bus resource [io 0x0000-0xffff]
<14:13:37.702> [ 2.141757] pci_bus 0000:00: root bus resource [mem 0x2040000000-0x207fffffff] (bus address [0x40000000-0x7fffffff])
<14:13:37.704> [ 2.152396] pci 0000:00:00.0: [1957:80c0] type 01 class 0x060400
<14:13:37.706> [ 2.158506] pci 0000:00:00.0: supports D1 D2
<14:13:37.708> [ 2.162813] pci 0000:00:00.0: PME# supported from D0 D1 D2 D3hot
<14:13:37.708> [ 2.170485] pci 0000:00:00.0: PCI bridge to [bus 01-ff]
<14:13:37.740> [ 2.175922] layerscape-pcie 3600000.pcie: host bridge /soc/pcie@3600000 ranges:
<14:13:37.743> [ 2.183314] layerscape-pcie 3600000.pcie: IO 0x3000010000..0x300001ffff -> 0x0000000000
<14:13:37.745> [ 2.191941] layerscape-pcie 3600000.pcie: MEM 0x3040000000..0x307fffffff -> 0x0040000000
<14:13:37.747> [ 2.200645] layerscape-pcie 3600000.pcie: PCI host bridge to bus 0001:00
<14:13:37.748> [ 2.207410] pci_bus 0001:00: root bus resource [bus 00-ff]
<14:13:37.750> [ 2.212946] pci_bus 0001:00: root bus resource [io 0x10000-0x1ffff] (bus address [0x0000-0xffff])
<14:13:37.784> [ 2.221990] pci_bus 0001:00: root bus resource [mem 0x3040000000-0x307fffffff] (bus address [0x40000000-0x7fffffff])
<14:13:37.800> [ 2.232624] pci 0001:00:00.0: [1957:80c0] type 01 class 0x060400
<14:13:37.800> [ 2.238724] pci 0001:00:00.0: supports D1 D2
<14:13:37.801> [ 2.243032] pci 0001:00:00.0: PME# supported from D0 D1 D2 D3hot
<14:13:37.804> [ 2.250651] pci 0001:00:00.0: PCI bridge to [bus 01-ff]
<14:13:37.806> [ 2.256644] EINJ: ACPI disabled.
<14:13:37.806> [ 2.264156] Bus freq driver module loaded
<14:13:37.808> [ 2.272511] Serial: 8250/16550 driver, 4 ports, IRQ sharing enabled
<14:13:37.839> [ 2.280233] printk: console [ttyS0] disabled
<14:13:37.863> [ 2.284580] 21c0500.serial: ttyS0 at MMIO 0x21c0500 (irq = 16, base_baud = 21875000) is a 16550A
<14:13:37.866> [ 2.293469] printk: console [ttyS0] enabled
<14:13:37.866> [ 2.293469] printk: console [ttyS0] enabled
<14:13:37.866> [ 2.301864] printk: bootconsole [uart8250] disabled
<14:13:37.869> [ 2.301864] printk: bootconsole [uart8250] disabled
<14:13:37.871> [ 2.311982] 21c0600.serial: ttyS1 at MMIO 0x21c0600 (irq = 16, base_baud = 21875000) is a 16550A
<14:13:37.871> [ 2.321085] SuperH (H)SCI(F) driver initialized
<14:13:37.873> [ 2.325920] msm_serial: driver initialized
<14:13:37.873> [ 2.331108] arm-smmu 5000000.iommu: probing hardware configuration...
<14:13:37.875> [ 2.337551] arm-smmu 5000000.iommu: SMMUv2 with:
<14:13:37.907> [ 2.342169] arm-smmu 5000000.iommu: stage 1 translation
<14:13:37.907> [ 2.347481] arm-smmu 5000000.iommu: stage 2 translation
<14:13:37.939> [ 2.352791] arm-smmu 5000000.iommu: nested translation
<14:13:37.939> [ 2.358016] arm-smmu 5000000.iommu: stream matching with 128 register groups
<14:13:37.943> [ 2.365153] arm-smmu 5000000.iommu: 64 context banks (0 stage-2 only)
<14:13:37.944> [ 2.371683] arm-smmu 5000000.iommu: Supported page sizes: 0x61311000
<14:13:37.945> [ 2.378124] arm-smmu 5000000.iommu: Stage-1: 48-bit VA -> 48-bit IPA
<14:13:37.947> [ 2.384565] arm-smmu 5000000.iommu: Stage-2: 48-bit IPA -> 48-bit PA
<14:13:37.949> [ 2.393824] cacheinfo: Unable to detect cache hierarchy for CPU 0
<14:13:37.949> [ 2.404174] brd: module loaded
<14:13:37.951> [ 2.412293] loop: module loaded
<14:13:37.951> [ 2.415619] pci-endpoint-test 0000:00:00.0: Adding to iommu group 0
<14:13:37.982> [ 2.422036] pci-endpoint-test 0001:00:00.0: Adding to iommu group 1
<14:13:38.000> [ 2.428933] megasas: 07.714.04.00-rc1
<14:13:38.002> [ 2.433397] imx ahci driver is registered.
<14:13:38.002> [ 2.437710] ahci-qoriq 3200000.sata: Adding to iommu group 2
<14:13:38.005> [ 2.443414] ahci-qoriq 3200000.sata: supply ahci not found, using dummy regulator
<14:13:38.006> [ 2.450967] ahci-qoriq 3200000.sata: supply phy not found, using dummy regulator
<14:13:38.008> [ 2.458390] ahci-qoriq 3200000.sata: supply target not found, using dummy regulator
<14:13:38.009> [ 2.466128] ahci-qoriq 3200000.sata: AHCI 0001.0301 32 slots 1 ports 6 Gbps 0x1 impl platform mode
<14:13:38.012> [ 2.475092] ahci-qoriq 3200000.sata: flags: 64bit ncq sntf pm clo only pmp fbs pio slum part ccc sds apst
<14:13:38.044> [ 2.485421] scsi host0: ahci-qoriq
<14:13:38.062> [ 2.489000] ata1: SATA max UDMA/133 mmio [mem 0x03200000-0x0320ffff] port 0x100 irq 26
<14:13:38.068> [ 2.497730] nand: device found, Manufacturer ID: 0x2c, Chip ID: 0xac
<14:13:38.069> [ 2.504086] nand: Micron MT29F4G08ABBDAH4
<14:13:38.069> [ 2.508095] nand: 512 MiB, SLC, erase size: 128 KiB, page size: 2048, OOB size: 64
<14:13:38.071> [ 2.515966] Bad block table found at page 262080, version 0x01
<14:13:38.072> [ 2.522338] Bad block table found at page 262016, version 0x01
<14:13:38.075> [ 2.532432] fsl,ifc-nand 530000000.nand: IFC NAND device at 0x530000000, bank 0
<14:13:38.077> [ 2.540785] spi-nor spi0.0: s25fs512s (65536 Kbytes)
<14:13:38.108> [ 2.548541] spi-nor spi0.1: s25fs512s (65536 Kbytes)
<14:13:38.124> [ 2.557758] libphy: Fixed MDIO Bus: probed
<14:13:38.124> [ 2.562747] tun: Universal TUN/TAP device driver, 1.6
<14:13:38.125> [ 2.568243] thunder_xcv, ver 1.0
<14:13:38.125> [ 2.571485] thunder_bgx, ver 1.0
<14:13:38.128> [ 2.574735] nicpf, ver 1.0
<14:13:38.128> [ 2.577850] libphy: Freescale XGMAC MDIO Bus: probed
<14:13:38.130> [ 2.588169] libphy: Freescale XGMAC MDIO Bus: probed
<14:13:38.132> [ 2.596366] libphy: Freescale XGMAC MDIO Bus: probed
<14:13:38.165> [ 2.601799] libphy: Freescale XGMAC MDIO Bus: probed
<14:13:38.165> [ 2.607908] libphy: Freescale XGMAC MDIO Bus: probed
<14:13:38.194> [ 2.613798] Freescale FM module, FMD API version 21.1.0
<14:13:38.196> [ 2.619119] Freescale FM Ports module
<14:13:38.196> [ 2.622779] fsl_mac: fsl_mac: FSL FMan MAC API based driver
<14:13:38.198> [ 2.628416] fsl_dpa: FSL DPAA Ethernet driver
<14:13:38.201> [ 2.632822] fsl_advanced: FSL DPAA Advanced drivers:
<14:13:38.201> [ 2.637784] fsl_proxy: FSL DPAA Proxy initialization driver
<14:13:38.203> [ 2.643401] fsl_oh: FSL FMan Offline Parsing port driver
<14:13:38.205> [ 2.649167] hclge is initializing
<14:13:38.208> [ 2.652493] hns3: Hisilicon Ethernet Network Driver for Hip08 Family - version
<14:13:38.209> [ 2.659714] hns3: Copyright (c) 2017 Huawei Corporation.
<14:13:38.209> [ 2.665049] e1000: Intel(R) PRO/1000 Network Driver
<14:13:38.211> [ 2.669924] e1000: Copyright (c) 1999-2006 Intel Corporation.
<14:13:38.213> [ 2.675695] e1000e: Intel(R) PRO/1000 Network Driver
<14:13:38.216> [ 2.680661] e1000e: Copyright(c) 1999 - 2015 Intel Corporation.
<14:13:38.248> [ 2.686605] igb: Intel(R) Gigabit Ethernet Network Driver
<14:13:38.267> [ 2.692001] igb: Copyright (c) 2007-2014 Intel Corporation.
<14:13:38.269> [ 2.697591] igbvf: Intel(R) Gigabit Virtual Function Network Driver
<14:13:38.272> [ 2.703856] igbvf: Copyright (c) 2009 - 2012 Intel Corporation.
<14:13:38.272> [ 2.709959] sky2: driver version 1.30
<14:13:38.274> [ 2.714222] usbcore: registered new interface driver r8152
<14:13:38.276> [ 2.719727] usbcore: registered new interface driver asix
<14:13:38.278> [ 2.725141] usbcore: registered new interface driver ax88179_178a
<14:13:38.278> [ 2.731543] VFIO - User Level meta-driver version: 0.3
<14:13:38.280> [ 2.737006] dwc3 3100000.usb3: Adding to iommu group 3
<14:13:38.281> [ 2.742704] dwc3 3110000.usb3: Adding to iommu group 4
<14:13:38.313> [ 2.749331] ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
<14:13:38.313> [ 2.755862] ehci-pci: EHCI PCI platform driver
<14:13:38.342> [ 2.760325] ehci-platform: EHCI generic platform driver
<14:13:38.352> [ 2.765614] ehci-orion: EHCI orion driver
<14:13:38.352> [ 2.769677] ehci-exynos: EHCI Exynos driver
<14:13:38.354> [ 2.773906] ohci_hcd: USB 1.1 'Open' Host Controller (OHCI) Driver
<14:13:38.356> [ 2.780093] ohci-pci: OHCI PCI platform driver
<14:13:38.358> [ 2.784556] ohci-platform: OHCI generic platform driver
<14:13:38.358> [ 2.789842] ohci-exynos: OHCI Exynos driver
<14:13:38.362> [ 2.794279] xhci-hcd xhci-hcd.0.auto: xHCI Host Controller
<14:13:38.363> [ 2.799775] xhci-hcd xhci-hcd.0.auto: new USB bus registered, assigned bus number 1
<14:13:38.363> [ 2.807498] xhci-hcd xhci-hcd.0.auto: hcc params 0x0220f66d hci version 0x100 quirks 0x0000000002010010
<14:13:38.365> [ 2.810047] ata1: SATA link down (SStatus 0 SControl 300)
<14:13:38.365> [ 2.816917] xhci-hcd xhci-hcd.0.auto: irq 24, io mem 0x03100000
<14:13:38.372> [ 2.828628] hub 1-0:1.0: USB hub found
<14:13:38.372> [ 2.832395] hub 1-0:1.0: 1 port detected
<14:13:38.375> [ 2.836491] xhci-hcd xhci-hcd.0.auto: xHCI Host Controller
<14:13:38.376> [ 2.841985] xhci-hcd xhci-hcd.0.auto: new USB bus registered, assigned bus number 2
<14:13:38.428> [ 2.849647] xhci-hcd xhci-hcd.0.auto: Host supports USB 3.0 SuperSpeed
<14:13:38.428> [ 2.856201] usb usb2: We don't know the algorithms for LPM for this host, disabling LPM.
<14:13:38.477> [ 2.864557] hub 2-0:1.0: USB hub found
<14:13:38.477> [ 2.868319] hub 2-0:1.0: 1 port detected
<14:13:38.479> [ 2.872594] usbcore: registered new interface driver uas
<14:13:38.480> [ 2.877948] usbcore: registered new interface driver usb-storage
<14:13:38.480> [ 2.885816] ftm-alarm 2800000.timer: registered as rtc1
<14:13:38.482> [ 2.891531] i2c /dev entries driver
<14:13:38.484> [ 2.896554] i2c i2c-0: Added multiplexed i2c bus 1
<14:13:38.484> [ 2.901455] i2c i2c-0: Added multiplexed i2c bus 2
<14:13:38.485> [ 2.906476] i2c i2c-0: Added multiplexed i2c bus 3
<14:13:38.487> [ 2.911571] i2c i2c-0: Added multiplexed i2c bus 4
<14:13:38.487> [ 2.916481] i2c i2c-0: Added multiplexed i2c bus 5
<14:13:38.490> [ 2.921385] i2c i2c-0: Added multiplexed i2c bus 6
<14:13:38.492> [ 2.926294] i2c i2c-0: Added multiplexed i2c bus 7
<14:13:38.492> [ 2.931195] i2c i2c-0: Added multiplexed i2c bus 8
<14:13:38.493> [ 2.935994] pca954x 0-0077: registered 8 multiplexed busses for I2C mux pca9547
<14:13:38.495> [ 2.952595] sp805-wdt c000000.wdt: registration successful
<14:13:38.496> [ 2.958202] sp805-wdt c010000.wdt: registration successful
<14:13:38.526> [ 2.963800] sp805-wdt c020000.wdt: registration successful
<14:13:38.562> [ 2.969394] sp805-wdt c030000.wdt: registration successful
<14:13:38.562> [ 2.974987] sp805-wdt c100000.wdt: registration successful
<14:13:38.574> [ 2.980590] sp805-wdt c110000.wdt: registration successful
<14:13:38.576> [ 2.986249] sp805-wdt c120000.wdt: registration successful
<14:13:38.578> [ 2.991845] sp805-wdt c130000.wdt: registration successful
<14:13:38.580> [ 2.998851] qoriq-cpufreq qoriq-cpufreq: Freescale QorIQ CPU frequency scaling driver
<14:13:38.582> [ 3.007725] sdhci: Secure Digital Host Controller Interface driver
<14:13:38.584> [ 3.013907] sdhci: Copyright(c) Pierre Ossman
<14:13:38.584> [ 3.018576] Synopsys Designware Multimedia Card Interface Driver
<14:13:38.584> [ 3.025150] sdhci-pltfm: SDHCI platform and OF driver helper
<14:13:38.586> [ 3.031362] sdhci-esdhc 2140000.esdhc: Adding to iommu group 5
<14:13:38.588> [ 3.037378] ledtrig-cpu: registered to indicate activity on CPUs
<14:13:38.591> [ 3.044189] SMCCC: SOC_ID: ARCH_SOC_ID not implemented, skipping ....
<14:13:38.591> [ 3.051481] usbcore: registered new interface driver usbhid
<14:13:38.593> [ 3.057084] usbhid: USB HID core driver
<14:13:38.626> [ 3.061644] No fsl,qman node
<14:13:38.626> [ 3.063958] mmc0: SDHCI controller on 2140000.esdhc [2140000.esdhc] using ADMA 64-bit
<14:13:38.645> [ 3.064579] Freescale USDPAA process driver
<14:13:38.656> [ 3.076583] fsl-usdpaa: no region found
<14:13:38.656> [ 3.080434] Freescale USDPAA process IRQ driver
<14:13:38.661> [ 3.087495] optee: probing for conduit method.
<14:13:38.661> [ 3.091964] optee: api uid mismatch
<14:13:38.680> [ 3.095463] optee: probe of firmware:optee failed with error -22
<14:13:38.683> [ 3.105334] NET: Registered protocol family 26
<14:13:38.683> [ 3.109830] u32 classifier
<14:13:38.685> [ 3.112565] input device check on
<14:13:38.685> [ 3.116238] Actions configured
<14:13:38.688> [ 3.120283] Initializing XFRM netlink socket
<14:13:38.688> [ 3.124639] NET: Registered protocol family 10
<14:13:38.691> [ 3.129521] Segment Routing with IPv6
<14:13:38.693> [ 3.133250] sit: IPv6, IPv4 and MPLS over IPv4 tunneling driver
<14:13:38.694> [ 3.139498] NET: Registered protocol family 17
<14:13:38.694> [ 3.143954] NET: Registered protocol family 15
<14:13:38.694> [ 3.145150] mmc0: new high speed SDHC card at address 59b4
<14:13:38.694> [ 3.148433] Bridge firewalling registered
<14:13:38.694> [ 3.154614] mmcblk0: mmc0:59b4 USD00 14.7 GiB
<14:13:38.702> [ 3.158055] 8021q: 802.1Q VLAN Support v1.8
<14:13:38.702> [ 3.163620] mmcblk0: p1 p2 p3 p4
<14:13:38.705> [ 3.166587] lib80211: common routines for IEEE802.11 drivers
<14:13:38.737> [ 3.175586] 9pnet: Installing 9P2000 support
<14:13:38.747> [ 3.179880] tsn generic netlink module v1 init...
<14:13:38.747> [ 3.184640] Key type dns_resolver registered
<14:13:38.747> [ 3.189340] registered taskstats version 1
<14:13:38.747> [ 3.193443] Loading compiled-in X.509 certificates
<14:13:38.752> [ 3.199150] Btrfs loaded, crc32c=crc32c-generic
<14:13:38.753> [ 3.205788] fsl_mc_dprc dprc.1: Adding to iommu group 6
<14:13:38.778> [ 3.237796] fsl_mc_allocator dpbp.1: Adding to iommu group 6
<14:13:38.780> [ 3.244573] fsl_mc_allocator dpmcp.17: Adding to iommu group 6
<14:13:38.811> [ 3.251010] fsl_mc_allocator dpmcp.16: Adding to iommu group 6
<14:13:38.830> [ 3.257445] fsl_mc_allocator dpmcp.15: Adding to iommu group 6
<14:13:38.831> [ 3.263893] fsl_mc_allocator dpmcp.14: Adding to iommu group 6
<14:13:38.835> [ 3.270328] fsl_mc_allocator dpmcp.13: Adding to iommu group 6
<14:13:38.835> [ 3.276764] fsl_mc_allocator dpmcp.12: Adding to iommu group 6
<14:13:38.836> [ 3.283198] fsl_mc_allocator dpmcp.11: Adding to iommu group 6
<14:13:38.839> [ 3.289634] fsl_mc_allocator dpmcp.10: Adding to iommu group 6
<14:13:38.839> [ 3.296078] fsl_mc_allocator dpmcp.9: Adding to iommu group 6
<14:13:38.842> [ 3.302426] fsl_mc_allocator dpmcp.8: Adding to iommu group 6
<14:13:38.873> [ 3.308774] fsl_mc_allocator dpmcp.7: Adding to iommu group 6
<14:13:38.873> [ 3.315121] fsl_mc_allocator dpmcp.6: Adding to iommu group 6
<14:13:38.902> [ 3.321469] fsl_mc_allocator dpmcp.5: Adding to iommu group 6
<14:13:38.903> [ 3.327817] fsl_mc_allocator dpmcp.4: Adding to iommu group 6
<14:13:38.905> [ 3.334167] fsl_mc_allocator dpmcp.3: Adding to iommu group 6
<14:13:38.907> [ 3.340529] fsl_mc_allocator dpmcp.2: Adding to iommu group 6
<14:13:38.907> [ 3.346877] fsl_mc_allocator dpmcp.1: Adding to iommu group 6
<14:13:38.909> [ 3.352726] fsl_mc_allocator dpcon.1: Adding to iommu group 6
<14:13:38.911> [ 3.358574] fsl_dpaa2_eth dpni.0: Adding to iommu group 6
<14:13:38.944> [ 3.382374] fsl_dpaa2_mac dpmac.10: Adding to iommu group 6
<14:13:38.944> [ 3.392507] fsl_dpaa2_mac dpmac.9: Adding to iommu group 6
<14:13:38.969> [ 3.402669] fsl_dpaa2_mac dpmac.8: Adding to iommu group 6
<14:13:38.971> [ 3.413120] fsl_dpaa2_mac dpmac.7: Adding to iommu group 6
<14:13:38.974> [ 3.423657] fsl_dpaa2_mac dpmac.6: Adding to iommu group 6
<14:13:38.974> [ 3.434263] fsl_dpaa2_mac dpmac.5: Adding to iommu group 6
<14:13:38.977> [ 3.440497] fsl_dpaa2_mac dpmac.4: Adding to iommu group 6
<14:13:39.010> [ 3.451930] fsl_dpaa2_mac dpmac.3: Adding to iommu group 6
<14:13:39.010> [ 3.462379] fsl_dpaa2_mac dpmac.2: Adding to iommu group 6
<14:13:39.015> [ 3.472981] fsl_dpaa2_mac dpmac.1: Adding to iommu group 6
<14:13:39.018> [ 3.483637] fsl_dpaa2_ptp dprtc.0: Adding to iommu group 6
<14:13:39.050> [ 3.491601] ptp_qoriq: device tree node missing required elements, try automatic configuration
<14:13:39.063> [ 3.500382] pps pps0: new PPS source ptp0
<14:13:39.064> [ 3.505604] fsl_mc_dpio dpio.8: Adding to iommu group 6
<14:13:39.064> [ 3.514463] fsl_mc_dpio dpio.8: probed
<14:13:39.064> [ 3.519826] fsl_mc_dpio dpio.7: Adding to iommu group 6
<14:13:39.070> [ 3.528674] fsl_mc_dpio dpio.7: probed
<14:13:39.070> [ 3.534046] fsl_mc_dpio dpio.6: Adding to iommu group 6
<14:13:39.103> [ 3.542895] fsl_mc_dpio dpio.6: probed
<14:13:39.103> [ 3.548266] fsl_mc_dpio dpio.5: Adding to iommu group 6
<14:13:39.108> [ 3.557106] fsl_mc_dpio dpio.5: probed
<14:13:39.108> [ 3.562581] fsl_mc_dpio dpio.4: Adding to iommu group 6
<14:13:39.111> [ 3.571484] fsl_mc_dpio dpio.4: probed
<14:13:39.113> [ 3.576856] fsl_mc_dpio dpio.3: Adding to iommu group 6
<14:13:39.143> [ 3.585700] fsl_mc_dpio dpio.3: probed
<14:13:39.183> [ 3.591063] fsl_mc_dpio dpio.2: Adding to iommu group 6
<14:13:39.183> [ 3.599919] fsl_mc_dpio dpio.2: probed
<14:13:39.190> [ 3.605274] fsl_mc_dpio dpio.1: Adding to iommu group 6
<14:13:39.192> [ 3.610514] fsl_mc_dprc dprc.1: No more resources of type dpmcp left
<14:13:39.192> [ 3.620086] fsl_mc_dprc dprc.1: DPRC device bound to driver
<14:13:39.194> [ 3.625805] pcieport 0000:00:00.0: PME: Signaling with IRQ 106
<14:13:39.196> [ 3.631810] pcieport 0001:00:00.0: PME: Signaling with IRQ 107
<14:13:39.198> [ 3.637818] fsl_mc_dprc dprc.1: No more resources of type dpmcp left
<14:13:39.201> [ 3.644746] fsl_mc_dprc dprc.1: No more resources of type dpmcp left
<14:13:39.202> [ 3.651247] fsl_mc_dprc dprc.1: No more resources of type dpmcp left
<14:13:39.204> [ 3.658220] fsl_mc_dprc dprc.1: No more resources of type dpmcp left
<14:13:51.480> [ 15.943957] ALSA device list:
<14:13:51.500> [ 15.946941] No soundcards found.
<14:13:51.500> [ 15.950705] Waiting 1 sec before mounting root device...
<14:15:31.352> [ 115.816585] VFS: Unable to mount root fs via NFS.
<14:15:31.364> [ 115.821398] devtmpfs: mounted
<14:15:31.394> [ 115.828695] Freeing unused kernel memory: 6656K
<14:15:31.394> [ 115.839997] Run /sbin/init as init process
<14:15:31.399> [ 115.844328] Run /etc/init as init process
<14:15:31.399> [ 115.848428] Run /bin/init as init process
<14:15:31.401> [ 115.852512] Run /bin/sh as init process
<14:15:31.407> [ 115.856388] Kernel panic - not syncing: No working init found. Try passing init= option to kernel. See Linux Documentation/admi
n-guide/init.rst for guidance.
<14:15:31.407> [ 115.870556] CPU: 0 PID: 1 Comm: swapper/0 Not tainted 5.10.35 #1
<14:15:31.437> [ 115.876557] Hardware name: LS1088ARDB-PB Board (DT)
<14:15:31.468> [ 115.881428] Call trace:
<14:15:31.468> [ 115.883872] dump_backtrace+0x0/0x1a8
<14:15:31.468> [ 115.887529] show_stack+0x18/0x68
<14:15:31.468> [ 115.890839] dump_stack+0xd0/0x12c
<14:15:31.470> [ 115.894235] panic+0x16c/0x334
<14:15:31.470> [ 115.897284] kernel_init+0xfc/0x118
<14:15:31.470> [ 115.900765] ret_from_fork+0x10/0x34
<14:15:31.470> [ 115.904338] SMP: stopping secondary CPUs
<14:15:31.476> [ 115.908265] Kernel Offset: 0x502ba6800000 from 0xffff800010000000
<14:15:31.491> [ 115.914351] PHYS_OFFSET: 0xffffc25200000000
<14:15:31.491> [ 115.918527] CPU features: 0x0240002,2080200c
<14:15:31.493> [ 115.922789] Memory Limit: none
<14:15:31.493> [ 115.925843] ---[ end Kernel panic - not syncing: No working init found. Try passing init= option to kernel. See Linux Documenta
tion/admin-guide/init.rst for guidance. ]---

You may note that ATF and u-boot are "mine", but tese are simply my compilations of the original sources. And they seems to work...:-(

0 件の賞賛
返信