Hello dear IMX support team,
I was wondering how to add support for the sn65dsi83 bridge on a IMX8MQ based board. This is the old device tree that used to work on the Linux IMX 5.4 kernel.
It seems that I'm missing something because I get the following errors from the output of journalctl.
imx-dcss 32e00000.display-controller: IRQ ctxld not found
imx-dcss 32e00000.display-controller: submodules initialization failed
nwl-dsi 30a00000.mipi_dsi: [drm:nwl_dsi_probe] Using LCDIF as input source
Maybe I need to also specify a missing endpoint.
[ 1.933819] nwl-dsi 30a00000.mipi-dsi: [drm:nwl_dsi_probe] *ERROR* No valid input endpoint found
[ 1.942685] nwl-dsi: probe of 30a00000.mipi-dsi failed with error -22
I saw here an example on how to setup the device tree. I saw that mine is similar with the exemption that I'm missing a port parameter. Seems that the definition changed on the new kernel source.
This is the port definition that I'm missing from my device tree. The issue here is that I don't know where &panel_in_lvds is coming from and where or how to I define one. I'm using a G1211XN01 Panel.
port@2 {
reg = <2>;
endpoint {
remote-endpoint = <&panel_in_lvds>;
};
Here is the device tree that I currently have.
/*
* Copyright 2017 NXP
*
* This program is free software; you can redistribute it and/or
* modify it under the terms of the GNU General Public License
* as published by the Free Software Foundation; either version 2
* of the License, or (at your option) any later version.
*
* This program is distributed in the hope that it will be useful,
* but WITHOUT ANY WARRANTY; without even the implied warranty of
* MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the
* GNU General Public License for more details.
*/
#include "imx8mq-itx-p-c444.dts"
&irqsteer {
status = "okay";
};
/delete-node/ &hdmi;
/ {
bl: backlight {
compatible = "pwm-backlight";
pwms = <&pwm1 0 5000000 0>;
brightness-levels = < 0 1 2 3 4 5 6 7 8 9
10 11 12 13 14 15 16 17 18 19
20 21 22 23 24 25 26 27 28 29
30 31 32 33 34 35 36 37 38 39
40 41 42 43 44 45 46 47 48 49
50 51 52 53 54 55 56 57 58 59
60 61 62 63 64 65 66 67 68 69
70 71 72 73 74 75 76 77 78 79
80 81 82 83 84 85 86 87 88 89
90 91 92 93 94 95 96 97 98 99
100>;
default-brightness-level = <80>;
status = "okay";
};
sound-hdmi {
status = "disabled";
};
};
&lcdif {
status = "disabled";
};
&dcss {
status = "okay";
// disp-dev = "mipi_disp";
clocks = <&clk IMX8MQ_CLK_DISP_APB_ROOT>,
<&clk IMX8MQ_CLK_DISP_AXI_ROOT>,
<&clk IMX8MQ_CLK_DISP_RTRM_ROOT>,
<&clk IMX8MQ_CLK_DC_PIXEL>,
<&clk IMX8MQ_CLK_DUMMY>,
<&clk IMX8MQ_CLK_DISP_DTRC>;
clock-names = "apb", "axi", "rtrm", "pix", "pix_out", "dtrc";
assigned-clocks = <&clk IMX8MQ_CLK_DC_PIXEL>,
<&clk IMX8MQ_CLK_DISP_AXI>,
<&clk IMX8MQ_CLK_DISP_RTRM>,
<&clk IMX8MQ_VIDEO_PLL1_REF_SEL>,
<&clk IMX8MQ_VIDEO_PLL1>;
assigned-clock-parents = <&clk IMX8MQ_VIDEO_PLL1_OUT>,
<&clk IMX8MQ_SYS1_PLL_800M>,
<&clk IMX8MQ_SYS1_PLL_800M>,
<&clk IMX8MQ_CLK_25M>;
assigned-clock-rates = <600000000>,
<800000000>,
<0>,
<400000000>,
<599999999>;
port@0 {
dcss_out: endpoint {
remote-endpoint = <&mipi_dsi_in>;
};
};
};
&dphy {
status = "okay";
};
&mipi_dsi {
status = "okay";
/*
assigned-clocks = <&clk IMX8MQ_CLK_DSI_PHY_REF>,
<&clk IMX8MQ_CLK_DSI_CORE>,
<&clk IMX8MQ_VIDEO_PLL1_REF_SEL>,
<&clk IMX8MQ_VIDEO_PLL1>;
assigned-clock-parents = <&clk IMX8MQ_VIDEO_PLL1_OUT>,
<&clk IMX8MQ_SYS1_PLL_266M>,
<&clk IMX8MQ_CLK_25M>;
assigned-clock-rates = <24000000>,
<266000000>,
<0>,
<599999999>;
*/
ports {
#address-cells = <1>;
#size-cells = <0>;
port@0 {
reg = <0>;
mipi_dsi_in: endpoint {
remote-endpoint = <&dcss_out>;
};
};
port@1 {
reg = <1>;
mipi_dsi_out: endpoint {
remote-endpoint = <&lvds_bridge_in>;
};
};
};
};
&i2c3 {
dsi_lvds_bridge: sn65dsi83@2c {
compatible = "ti,sn65dsi83";
reg = <0x2c>;
ti,dsi-lanes = <4>;
ti,lvds-format = <1>;
ti,lvds-bpp = <24>;
ti,width-mm = <245>;
ti,height-mm = <184>;
enable-gpios = <&gpio3 23 GPIO_ACTIVE_HIGH>;
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_lvds_bridge_en>;
status = "okay";
display-timings {
native-mode = <&timing0>;
timing0: 1024x768_60Hz {
clock-frequency = <65000000>;
hactive = <1024>;
vactive = <768>;
hback-porch = <156>;
hfront-porch = <156>;
vback-porch = <16>;
vfront-porch = <16>;
hsync-len = <8>;
vsync-len = <6>;
de-active = <1>;
};
};
port@0 {
lvds_bridge_in: endpoint {
remote-endpoint = <&mipi_dsi_out>;
};
};
};
};
lvds_backlight: &pwm1 {
status = "okay";
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_backligth_pwm1>;
};
&iomuxc {
pinctrl_backligth_pwm1: backligth_pwm1 {
fsl,pins = <
/* BCKLT_PWM_3V3 */
MX8MQ_IOMUXC_SPDIF_EXT_CLK_PWM1_OUT 0x16
/* BCKLT_EN_3V3 */
MX8MQ_IOMUXC_SPDIF_TX_GPIO5_IO3 0x59
/* 12V_EN */
MX8MQ_IOMUXC_NAND_CE1_B_GPIO3_IO2 0x59
>;
};
/* Use the LVDS bridge EN Pin for the SN65DSI83 Reset */
pinctrl_lvds_bridge_en: lvds_bridge_en {
fsl,pins = <
/* LVDS_EN_1V8 */
MX8MQ_IOMUXC_SAI5_RXD2_GPIO3_IO23 0x16
/* LVDS_IRQ_1V8to3V3 */
MX8MQ_IOMUXC_SAI5_RXD3_GPIO3_IO24 0x16
/* SEL68_3V3 */
MX8MQ_IOMUXC_SAI5_RXD1_GPIO3_IO22 0x16
>;
};
};
Thanks.