MMU Level 3 table configuration on s32g274a a53 core

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MMU Level 3 table configuration on s32g274a a53 core

ソリューションへジャンプ
1,574件の閲覧回数
Greenhal
Contributor II

Hello Experts,

I have a problem with establishing the level 3 table in MMU for cortex-a53 in s32g274a processor. Level 1 and Level2 table works as expected but I need a 4KB memory block for my project. Below is the code that I wrote to configure the mmu. Could someone look at what is wrongly set so that the level 3 table is not configured correctly?  

MOV x0, #0x44 /* Inner/outer cacheable WB */
MSR mair_el3, x0
/* Invalidate TLBs at the current exception level */
TLBI alle3

/* RES1
RES1
PS 40-bit
ORGN0 outer WB no WA cacheable
IRGN0 inner WB no WA cacheable
T0SZ 39-bit region size */
LDR x0, =(1 << 31) | (1 << 23) | (2 << 16) | (3 << 10) | (3 << | 25
MSR tcr_el3, x0

/* Page table setup */

LDR x1, =ttb // Address of L1 table

//0x0000,0000 - 0x3FFF,FFFF
LDR x2, =ttb1 // Get address of L2 table
MOV x0, #0x03 // Entry template for pointer to next level table
ORR x0, x0, x2 // Combine template with L2 table Base address
STR x0, [x1]

//0x4000,0000 - 0x7FFF,FFFF
MOV x0, #0x405 // Entry template

ORR x0, x0, #0x40000000 // 'OR' template with base physical address
STR x0, [x1, #8]


LDR x1, =ttb1 // Address of L2 table

//0x0000,0000 - 0x2000,0000
MOV x0, #0x401
MOV x2, #0x100
1:
STR x0, [x1], #8
ADD x0, x0, #0x200000 // Increment the physical address field
SUB x2, x2, #1
CBNZ x2, 1b

//0x2000,0000 - 0x3400,0000 (Fault)
MOV x0, #0x0
ORR x0, x0, #0x20000000 // 'OR' template with base physical address
MOV x2, #0xA0
1:
STR x0, [x1], #8
ADD x0, x0, #0x200000 // Increment the physical address field
SUB x2, x2, #1
CBNZ x2, 1b


//0x3400,0000 - 0x3480,0000 (SDRAM)

mov x0, #0x401
MOV x6, #0x34000000
ORR x0, x0, x6 // 'OR' template with base physical address
MOV x2, #2
1:
STR x0, [x1], #8
ADD x0, x0, #0x200000 // Increment the physical address field
SUB x2, x2, #1
CBNZ x2, 1b

 

LDR x2, =ttb2 // Get address of L3 table
MOV x0, #0x03 // Entry template for pointer to next level table
ORR x0, x0, x2 // Combine template with L3 table
STR x0, [x1]

MOV x0, #0x405 // Entry template

MOV x6, #0x34600000
ORR x0, x0, x6 // 'OR' template with base physical address
STR x0, [x1, #8]


LDR x1, =ttb2 // Address of L3 table

//0x3440,0000 - 0x3460,0000
MOV x0, #0x401
MOV x6, #0x34400000
ORR x0, x0, x6 // 'OR' template with base physical address
MOV x2, #0x200
1:
STR x0, [x1], #8
ADD x0, x0, #0x1000 // Increment the physical address field
SUB x2, x2, #1
CBNZ x2, 1b
DSB SY


/* Ensure all translation table writes have drained into memory,
the TLB invalidation is complete,
and translation register writes are committed before enabling the MMU */
DSB ISH
ISB
LDR x0, =ttb // Address of L1 table
MSR ttbr0_el3, x0 // set TTBR

MRS x0, S3_1_c15_c2_1 // cpuectlr_el1
ORR x0, x0, #0x40
MSR S3_1_c15_c2_1, x0


MRS x0, sctlr_el3
bic x0, x0, #(1 << 1) /* clear A, disable alignment fault check */
/* I enable instruction cache
C enable data and unified caches
M enable EL3 MMU */
LDR x1, =(1 << 12) | (1 << 2) | 1
ORR x0, x0, x1 /* set bits */
MSR sctlr_el3, x0
/* Ensure the MMU enable takes effect immediately */
ISB

タグ(1)
0 件の賞賛
返信
1 解決策
1,554件の閲覧回数
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

This seems to be related directly to the A53 architecture, which might be supported from ARM support team, rather than the S32G team. Help us sending this inquiry to the ARM support team, for them to provide better support than the one we could provide. We do apologize.

Please, let us know.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,555件の閲覧回数
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

This seems to be related directly to the A53 architecture, which might be supported from ARM support team, rather than the S32G team. Help us sending this inquiry to the ARM support team, for them to provide better support than the one we could provide. We do apologize.

Please, let us know.

0 件の賞賛
返信