Kinetis ADC1 Channel 19

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Kinetis ADC1 Channel 19

1,796件の閲覧回数
stechsc
Contributor I

Hi,

I'm using PE to set up the ADC on the Kinetis MK40DX256ZVMD10.  When I select ADC1, Channel 19, the Component Inspector claims that the "Target CPU does not contain peripheral of this type".  However, the reference manual indicates otherwise, and that Channel 19 uses input pin ADC1_DM0.  I also tried this with a K10 and a K60 part selected, and got the same result.  Has anyone out there seen this?  Is there any way to configure ADC Channel 19 using PE?  

 

I am using CW 10.2.

 

Thanks.

ラベル(1)
タグ(1)
0 件の賞賛
返信
2 返答(返信)

1,505件の閲覧回数
ProcessorExpert
Senior Contributor III

Hello,

 

we are analyzing the problem. I think that I should have the answer, wokraround or hot-fix for you soon.

 

best regards
Vojtech Filip
Processor Expert Support Team


 

 

0 件の賞賛
返信

1,505件の閲覧回数
ProcessorExpert
Senior Contributor III

Hello,

 

we will prepare a hot-fix of this problem. Could you please confirm that your are using CW V10.2 or CW V10.2 installed together with CW V10.2 Update?

 

best regards
Vojtech Filip
Processor Expert Support Team

0 件の賞賛
返信