Kinetis ADC1 Channel 19

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Kinetis ADC1 Channel 19

1,891 次查看
stechsc
Contributor I

Hi,

I'm using PE to set up the ADC on the Kinetis MK40DX256ZVMD10.  When I select ADC1, Channel 19, the Component Inspector claims that the "Target CPU does not contain peripheral of this type".  However, the reference manual indicates otherwise, and that Channel 19 uses input pin ADC1_DM0.  I also tried this with a K10 and a K60 part selected, and got the same result.  Has anyone out there seen this?  Is there any way to configure ADC Channel 19 using PE?  

 

I am using CW 10.2.

 

Thanks.

标签 (1)
标记 (1)
0 项奖励
回复
2 回复数

1,600 次查看
ProcessorExpert
Senior Contributor III

Hello,

 

we are analyzing the problem. I think that I should have the answer, wokraround or hot-fix for you soon.

 

best regards
Vojtech Filip
Processor Expert Support Team


 

 

0 项奖励
回复

1,600 次查看
ProcessorExpert
Senior Contributor III

Hello,

 

we will prepare a hot-fix of this problem. Could you please confirm that your are using CW V10.2 or CW V10.2 installed together with CW V10.2 Update?

 

best regards
Vojtech Filip
Processor Expert Support Team

0 项奖励
回复