K60 USB Module - clock requirement

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

K60 USB Module - clock requirement

Jump to solution
2,601 Views
rc
Contributor I

I've done some searching in the forums and the help archives, but have not been able to confirm whether a 48MHz (or higher) clock is required to use the K60 USB module.

Currently I plan on using an 8MHz crystal for the system clock (EXTAL input on the K60), can I use this to internally generate the 48MHz required for USB?

Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
2,275 Views
MVa
NXP Employee
NXP Employee

Hi,

  USB FS module requires 48 MHz clock. See chapter 5.7.7 USB FS OTG Controller clocking in the reference manual (or attached picture).

One possible clock setting of the CPU component is shown in attached screenshot.

 

Best Regards

MVa

 

View solution in original post

0 Kudos
Reply
2 Replies
2,276 Views
MVa
NXP Employee
NXP Employee

Hi,

  USB FS module requires 48 MHz clock. See chapter 5.7.7 USB FS OTG Controller clocking in the reference manual (or attached picture).

One possible clock setting of the CPU component is shown in attached screenshot.

 

Best Regards

MVa

 

0 Kudos
Reply
2,275 Views
rcallagh
Contributor I

Thanks!

0 Kudos
Reply