K60 USB Module - clock requirement

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

K60 USB Module - clock requirement

ソリューションへジャンプ
2,583件の閲覧回数
rc
Contributor I

I've done some searching in the forums and the help archives, but have not been able to confirm whether a 48MHz (or higher) clock is required to use the K60 USB module.

Currently I plan on using an 8MHz crystal for the system clock (EXTAL input on the K60), can I use this to internally generate the 48MHz required for USB?

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
2,257件の閲覧回数
MVa
NXP Employee
NXP Employee

Hi,

  USB FS module requires 48 MHz clock. See chapter 5.7.7 USB FS OTG Controller clocking in the reference manual (or attached picture).

One possible clock setting of the CPU component is shown in attached screenshot.

 

Best Regards

MVa

 

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,258件の閲覧回数
MVa
NXP Employee
NXP Employee

Hi,

  USB FS module requires 48 MHz clock. See chapter 5.7.7 USB FS OTG Controller clocking in the reference manual (or attached picture).

One possible clock setting of the CPU component is shown in attached screenshot.

 

Best Regards

MVa

 

0 件の賞賛
返信
2,257件の閲覧回数
rcallagh
Contributor I

Thanks!

0 件の賞賛
返信