K60 USB Module - clock requirement

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

K60 USB Module - clock requirement

跳至解决方案
2,554 次查看
rc
Contributor I

I've done some searching in the forums and the help archives, but have not been able to confirm whether a 48MHz (or higher) clock is required to use the K60 USB module.

Currently I plan on using an 8MHz crystal for the system clock (EXTAL input on the K60), can I use this to internally generate the 48MHz required for USB?

标签 (1)
标记 (1)
0 项奖励
回复
1 解答
2,228 次查看
MVa
NXP Employee
NXP Employee

Hi,

  USB FS module requires 48 MHz clock. See chapter 5.7.7 USB FS OTG Controller clocking in the reference manual (or attached picture).

One possible clock setting of the CPU component is shown in attached screenshot.

 

Best Regards

MVa

 

在原帖中查看解决方案

0 项奖励
回复
2 回复数
2,229 次查看
MVa
NXP Employee
NXP Employee

Hi,

  USB FS module requires 48 MHz clock. See chapter 5.7.7 USB FS OTG Controller clocking in the reference manual (or attached picture).

One possible clock setting of the CPU component is shown in attached screenshot.

 

Best Regards

MVa

 

0 项奖励
回复
2,228 次查看
rcallagh
Contributor I

Thanks!

0 项奖励
回复