Is PEx for TWR-K21D50M broken?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is PEx for TWR-K21D50M broken?

1,345 Views
bonzo
NXP Employee
NXP Employee

Using either PEx stand-alone or in CW10.4, PEx does not allow me to set the CPU frequency to 48MHz using 8MHz crystal with FEE.

Furthermore, using the BitIO LDD, there is no method for Toggling a bit.

0 Kudos
Reply
2 Replies

1,198 Views
bonzo
NXP Employee
NXP Employee

PEE mode works.   Thank you.

0 Kudos
Reply

1,198 Views
vfilip
NXP Employee
NXP Employee

Hello,

I assume that PEx is correct. BitIO_LDD provides NegVal method for toggling purposes. Please also do not forget to switch to the Expert mode in the Component Inspector view (right top part of this view).

Regarding to running on 48MHz from 8MHz crystal in FEE mode. Would be OK for you to run in PEE mode? I was able to select 48 MHz in this mode. However in FEE seems that the max is 40 MHz based on the provided input values.

Best regards

Vojtech Filip

Processor Expert Support Team