How to set hi-buad with PE?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to set hi-buad with PE?

ソリューションへジャンプ
3,577件の閲覧回数
zhongshen
Contributor III

Hi,

I have the problem to use uart with hi-baud with PE. When I use PE to config uart1, or uart2 the highest baud rate is 57600. If I set the buad rate with more than 57600, there is a error in the PE.  How to set hi-buad with PE? Thanks.

Here is the picture of the buad setting in PE:

buad.png

Robert

0 件の賞賛
返信
1 解決策
3,276件の閲覧回数
marek_neuzil
NXP Employee
NXP Employee

Hello,

In case you need clock configuration for a Freescale target board you can use a board support project that is configured according to available devices on the board including clock sources (e.g. crystal oscillator). When you create a new project select the board support. For example the FRDM-KL25Z target board, see below:

pastedImage_0.png

The new project contain 5 clock configuration and there is selected clockMan1_InitConfig4 by default (24MHz bus clock, 48MHz core clock; PLL Engaged External (PEE) mode of MCG).

pastedImage_1.png

When you add the fsl_uart component you will be able to select the 115200 baudrate (24MHz / 208 = 115384 baud). See the attached project.

Best regards,

Marek Neuzil


 

元の投稿で解決策を見る

0 件の賞賛
返信
8 返答(返信)
3,276件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Hi Robert,

the maximum baud depends on your clock settings. But as the dialog says, you can set a baud from 160 to 1310720. So simply enter e.g. 115200 as your baud value, and if this is possible, it will be set and used.

I hope this helps,

Erich

0 件の賞賛
返信
3,276件の閲覧回数
zhongshen
Contributor III

Hi Erich,

If I set the 115200 as baud rate, there is error:

buad1.png

by the way, if I set 1310720, PE can accept with no error. As following picture:

buad1.png

0 件の賞賛
返信
3,276件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Then you need to increase the CPU clock (resp. Bus clock) in the CPU component (e.g. using PEE).

I hope this helps,

Erich

0 件の賞賛
返信
3,276件の閲覧回数
zhongshen
Contributor III

Could you advise how to increase the CPU clock? What is PEE?

0 件の賞賛
返信
3,276件の閲覧回数
BlackNight
NXP Employee
NXP Employee

That depends to some extend to the device you are using:

Example for KL25Z:

http://mcuoneclipse.com/2012/10/07/tutorial-usb-cdc-with-the-kl25z-freedom-board/

(search for PEE)

Erich

0 件の賞賛
返信
3,276件の閲覧回数
zhongshen
Contributor III

Yes, I use KL25Z and KDS 3.0. I do not use codewarrior. The CPU component in KDS PE does not have clock configuration. There is only fsl_clock_manager which can not be changed. And I found a clockMan1 component which can set the clock, but so many parameters, I do not know which parameter can be changed for uart baud at 115200. Could you advise me? Many thanks.

clock.png

Best regards,

Robert

0 件の賞賛
返信
3,277件の閲覧回数
marek_neuzil
NXP Employee
NXP Employee

Hello,

In case you need clock configuration for a Freescale target board you can use a board support project that is configured according to available devices on the board including clock sources (e.g. crystal oscillator). When you create a new project select the board support. For example the FRDM-KL25Z target board, see below:

pastedImage_0.png

The new project contain 5 clock configuration and there is selected clockMan1_InitConfig4 by default (24MHz bus clock, 48MHz core clock; PLL Engaged External (PEE) mode of MCG).

pastedImage_1.png

When you add the fsl_uart component you will be able to select the 115200 baudrate (24MHz / 208 = 115384 baud). See the attached project.

Best regards,

Marek Neuzil


 

0 件の賞賛
返信
3,276件の閲覧回数
zhongshen
Contributor III

Hi Marek,

Thanks for you help!  Based on your project, I reconfigure the MCG setting and it can be set at hi-buad on UART.

Best regards,

Robert Shen

0 件の賞賛
返信