How to activate CLK_OUT with FlexBus

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to activate CLK_OUT with FlexBus

Jump to solution
1,569 Views
mentair
Contributor I

Hi,

I have activated FlexBus in the CPU component. However, in the generated Code, all relevant pins are initialized to their correct alternative function (5 in my case), except for the CLKOUT pin (PORTC_PCR3), which has no initialization in Cpu.c

Is there a trick to activate that output?

PE Version: 10.3.0

Device: MK60FN1M0VLQ12

Thanks,

Martin

Tags (1)
0 Kudos
Reply
1 Solution
1,450 Views
marek_neuzil
NXP Employee
NXP Employee

Hi Martin,

The CLKOUT pin control settings is availble in the CPU component in the Internal peripherals / System Integration Module / CLKOUT pin control. These properties are visible in the Advance or Expert view of Component Inspector window only, see the screenshot below:

CLKOUT properties on MK60FN1M0.png

Best Regards,

Marek Neuzil

View solution in original post

0 Kudos
Reply
1 Reply
1,451 Views
marek_neuzil
NXP Employee
NXP Employee

Hi Martin,

The CLKOUT pin control settings is availble in the CPU component in the Internal peripherals / System Integration Module / CLKOUT pin control. These properties are visible in the Advance or Expert view of Component Inspector window only, see the screenshot below:

CLKOUT properties on MK60FN1M0.png

Best Regards,

Marek Neuzil

0 Kudos
Reply