How to activate CLK_OUT with FlexBus

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to activate CLK_OUT with FlexBus

ソリューションへジャンプ
1,585件の閲覧回数
mentair
Contributor I

Hi,

I have activated FlexBus in the CPU component. However, in the generated Code, all relevant pins are initialized to their correct alternative function (5 in my case), except for the CLKOUT pin (PORTC_PCR3), which has no initialization in Cpu.c

Is there a trick to activate that output?

PE Version: 10.3.0

Device: MK60FN1M0VLQ12

Thanks,

Martin

タグ(1)
0 件の賞賛
返信
1 解決策
1,466件の閲覧回数
marek_neuzil
NXP Employee
NXP Employee

Hi Martin,

The CLKOUT pin control settings is availble in the CPU component in the Internal peripherals / System Integration Module / CLKOUT pin control. These properties are visible in the Advance or Expert view of Component Inspector window only, see the screenshot below:

CLKOUT properties on MK60FN1M0.png

Best Regards,

Marek Neuzil

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,467件の閲覧回数
marek_neuzil
NXP Employee
NXP Employee

Hi Martin,

The CLKOUT pin control settings is availble in the CPU component in the Internal peripherals / System Integration Module / CLKOUT pin control. These properties are visible in the Advance or Expert view of Component Inspector window only, see the screenshot below:

CLKOUT properties on MK60FN1M0.png

Best Regards,

Marek Neuzil

0 件の賞賛
返信